USA

Select your location

USA
 

Press

Content
xxx 2011-02-23

Case Study: Rexroth helps friction welder put a new spin on welding plastic parts

Case Study: Rexroth helps friction welder put a new spin on welding plastic parts

Eagle Technologies’ plastics power welder uses Rexroth drive, control and linear motion technology to give washing machine parts manufacturer better overall performance.

Eagle Technologies used Rexroth drive and control products, including IndraDyn servo motors and IndraMotion MLD integrated motion logic control, to help a major appliance parts fabricator reduce waste and downtime and achieve precise results.

The drive-based Rexroth IndraMotion MLD integrated motion logic control platform is a Sercos III Ethernet-based system used in the Eagle Technologies plastics spin welding machine (which welds parts together by using high-speed friction). This eliminates the need for a separate PLC and combines motion and PLC functions in a single automation platform. The motion logic controller works with Rexroth’s IndraDrive digital intelligent servo drives and IndraDyn S motors to drive the spin welder, and allows precise control of low-speed, high-torque spin motion. Using the Rexroth HMI, operators can apply a full menu of parameters for each welding operation: motion, positioning, force, power usage and more. Changes to parts configurations and welding parameters can be accomplished through the touchscreen, instead of reconfiguring the entire machine. Result: A dramatic reduction in wasted parts due to improper welds, and a huge increase in throughput and productivity.

Rexroth’s Safety on Board drive-based machine safety system uses Safe Motion technology to maximize operator safety in cases where the operator must reach into the weld area.

The machine’s spinning welding head moves along a set of Rexroth precision Ball Screws and Ball Rails®, allowing powerful compression without flexing, ensuring tight welds and minimizing damage to the parts.

Download the complete application story from the Bosch Rexroth Case Studies & Technical Papers web page.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and renewable energy.

As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2009 Bosch Rexroth, part of the Bosch Group, achieved sales of around $5.7 billion (4.1 billion Euro) with 34,200 employees.

Visit www.boschrexroth-us.com for more information.

 

Search press releases


Contact

Bosch Rexroth  Corporation
Prairie Stone Parkway 5150
60192 Hoffman Estates, IL
Phone: (847) 645-3728
Fax: (847) 645-3728