USA

Select your location

USA
 

Press

Content
xxx 2011-02-08

Rexroth's New TS5 Assembly Conveyor Transports Loads up to 660 lb.

Rexroth's New TS5 Assembly Conveyor Transports Loads up to 660 lb.

New TS5 conveyor expands Rexroth's modular assembly conveyor offering and introduces a new, heavy-duty transfer system to the market.

(Buchanan, MI – www.boschrexroth-us.com ) The new TS5 transfer system from Bosch Rexroth's Linear Motion and Assembly Technologies group introduces a new class of conveyor to the market. The system features an incredibly robust design, suitable for harsh production environments and heavy transport of loads up to 300 kg (660 lb.).

Rexroth's TS5 conveyors boast a highly energy efficient drive system and quiet, maintenance-free operation with a “king shaft” powered roller design that requires no lubrication, resulting in greater system uptime. The TS5 system can be configured to transport goods either on a workpiece pallet or directly on a continuous roller conveyor, and is available in three widths. Curves are separate, self-contained units that allow the system to branch off to the right or to the left to achieve a wide variety of conveyor system layouts.

Users can plan and implement a TS5 transfer system that is perfectly matched to the unique requirements of their application, thanks to Rexroth's comprehensive selection of conveyor system components: drive modules, workpiece pallets, roller sections, curves, diverters, positioning units and components for traffic control.

All TS5 components are included in Bosch Rexroth's MTpro software program so that customers can configure the system and generate a parts list automatically, considerably simplifying the entire planning process. All components are modular, preassembled and can be combined as needed using a single interface, allowing for easy system expansion or reconfiguration in the future. The TS5 is an economical choice thanks to low purchase, start-up, and operating costs throughout the life of the system.

TS5 conveyors extend Rexroth’s industry-leading TS family of modular conveyors, designed for a wide range of flexible assembly and material transport applications for both automated and manual assembly operations.

To learn more about Rexroth's new line of TS5 conveyors and to download a product brochure, visit www.boschrexroth-us.com/conveyors.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros in revenue in 2011.

To learn more, please visit www.boschrexroth-us.com

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innnovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com.

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com.

 

Search press releases


Contact

Kevin Gingerich
South Lakes Drive 14001
28273  Charlotte, NC
Phone: (704) 714-8594
kevin.gingerich@boschrexroth-us.com