xxx 2011-09-15

AATExpo 2011: Faster Automation Thanks to New Functions

AATExpo 2011: Faster Automation Thanks to New Functions

IndraLogic XLC offers new functions, fast real-time communication via Sercos III, and is ideal for a variety of applications.

(Hoffman Estates, IL – ) Rexroth’s IndraLogic XLC PLC family enables scalable, controller-based and embedded PC solutions in conjunction with the company’s latest IndraControl device platform. Industrial PC-based hardware variants will round off the device portfolio in 2011.

Rexroth advanced the PLC programming using state-of-the-art PLC kernel, IndraLogic 2G, integrated homogeneously into the company’s IndraWorks software tool and the multitasking runtime system. This allows users to take advantage of many new functions for creating modular software projects in an end-to-end overall system in less time than before. Functions include convenient editor tools, object orientation as an extension to IEC 61131-3, and comprehensive function libraries as well as fast compilers for efficient generation of machine codes. The modular GATcompact (Generic Application Template) project template simplifies the process of designing new machines with enhanced software quality while reducing effort considerably.

End-to-end communication between the controller and decentralized system peripherals, such as inputs and outputs or drives, takes place via real-time Ethernet Sercos III. Fast PLC cycles to 250 µs enable optimum response times for handling time-critical process signals. IndraLogic XLC controllers come with versatile motion control functions, integrated into the run-time systems, to enhance the previous IndraLogic systems.

With its motion control functionality, the XLC handles machine applications ranging from simple point-to-point motion to the synchronization of multiple axes that use Rexroth’s FlexProfile to integrate complex motion sequences. The graphical profile editor in the Rexroth IndraWorks software tool offers numerous offline and online functions for this purpose. Master and slave interfaces for PROFINET RT, PROFIBUS and EtherNet/IP are also available, in addition to Sercos III, for integrating into a wide range of communication networks.

Visit Bosch Rexroth at AATExpo 2011 in Chicago’s McCormick Place, booth 1308. For more information, please visit

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue ($6.8 billion) in 2010. To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros ($62.7 billion) in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Additional information can be accessed at,


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670