The IndraDrive Cs Economy version gives machine builders more flexibility when selecting a compact servo drive that delivers the right amount of functionality for their low-power applications.
The IndraDrive Cs Economy is a compact servo drive featuring Sercos III communication and multi-encoder interfaces to provide flexibility and value for low-power applications.
(Hoffman Estates, IL –www.boschrexroth-us.com/brc ) The Rexroth IndraDrive Cs Economy low-power servo drive features an extremely compact space-saving design, and open support of Sercos III communication bus, providing a cost-effective drive platform delivering just the right amount of functionality.
The IndraDrive Cs Economy is ideal for industries ranging from packaging, semiconductor and medical, to printing, converting, machine tool and metal forming – for small-size applications in a low-power range.
Designed to provide flexibility and just the right amount of power at a lower cost, the drive also has a multi-encoder interface supporting Hiperface®, EnDat 2.1 and 2.2, 1Vss, 5 V TTL, and Rexroth MSM and MSK servo motors.
The IndraDrive Cs Economy is part of the Rexroth advanced automation platform that supports the Sercos III interface for connecting machines, controls, drives, I/O, safety, and HMI which helps to lower the controls cost and simplify integration for OEMs, systems integrators and end users.
Adding functionality and overall cost savings, the compact IndraDrive Cs Economy can be equipped with Safety-On-Board features such as Safe Torque Off and Safe Brake Control for certifiable drive-based machine safety, eliminating the need for separate safety components.
The Economy version of the IndraDrive Cs comes with digital inputs and outputs plus an analog input on board, integrated brake resistor, and an intelligent operation panel with programming module function. For users requiring more power or additional protocols, Rexroth also offers a Universal model of the IndraDrive Cs.
Available in models ranging from 50 W up to 3.5 kW, the IndraDrive Cs dimensions measure 50 x 215 x 196 (mm) for one unit, and 70 x 268 x 196 (mm) for the larger unit. Maximum current ranges from 3A up to 28A, with a high overload range. This size range makes it optimal for packaging applications.
The IndraDrive Cs platform includes Rexroth MSM and MSK series AC servo motors ranging from 50 W up to 3.5kW continuous power with IP54 protection (MSM) or IP65 protection (MSK), multi-turn absolute encoder functionality, and optional holding brake.
Visit Bosch Rexroth at AATExpo 2011 in Chicago’s McCormick Place, booth 1308. For more information, please visit www.boschrexroth-us.com/indradrive-cs.
Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue ($6.8 billion) in 2010. To learn more, please visit www.boschrexroth-us.com
The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros ($62.7 billion) in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Additional information can be accessed at www.bosch.com, and www.bosch-press.com.
For more information please visit: www.boschrexroth-us.com
Susan Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com