xxx 2012-02-08

Rexroth’s IndraDrive Cs Economy Version Compact Servo Drive Provides Higher Value, More Flexibility for Low Power Machine Applications

Rexroth’s IndraDrive Cs Economy Version Compact Servo Drive Provides Higher Value, More Flexibility

The IndraDrive Cs Economy version gives machine builders more flexibility when selecting a compact servo drive that delivers the right amount of functionality for their low-power applications.

(Charlotte, NC– ) The Rexroth IndraDrive Cs Economy low-power servo drive features an extremely compact space-saving design, and open support of Sercos III communication bus, providing a cost-effective drive platform delivering just the right amount of functionality.

The IndraDrive Cs Economy is ideal for industries ranging from packaging, semiconductor and medical, to printing, converting, machine tool and metal forming – for small-size applications in a low-power range.

Designed to provide flexibility and just the right amount of power at a lower cost, the drive also has a multi-encoder interface supporting Hiperface®, EnDat 2.1 and 2.2, 1Vss, 5 V TTL, and Rexroth MSM and MSK servo motors.

The IndraDrive Cs Economy is part of the Rexroth advanced automation platform that supports the Sercos III interface for connecting machines, controls, drives, I/O, safety, and HMI which helps to lower the controls cost and simplify integration for OEMs, systems integrators and end users.

Adding functionality and overall cost savings, the compact IndraDrive Cs Economy can be equipped with Safety-On-Board features such as Safe Torque Off and Safe Brake Control for certifiable drive-based machine safety, eliminating the need for separate safety components.

The Economy version of the IndraDrive Cs comes with digital inputs and outputs plus an analog input on board, integrated brake resistor, and an intelligent operation panel with programming module function. For users requiring more power or additional protocols, Rexroth also offers a Universal model of the IndraDrive Cs.

Available in models ranging from 50 W up to 3.5 kW, the IndraDrive Cs dimensions measure 50 x 215 x 196 (mm) for one unit, and 70 x 268 x 196 (mm) for the larger unit. Maximum current ranges from 3A up to 28A, with a high overload range. This size range makes it optimal for packaging applications.

The IndraDrive Cs platform includes Rexroth MSM and MSK series AC servo motors ranging from 50 W up to 3.5kW continuous power with IP54 protection (MSM) or IP65 protection (MSK), multi-turn absolute encoder functionality, and optional holding brake.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros in revenue in 2011.

To learn more, please visit

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innnovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit .

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at and .


Search press releases


Bosch Rexroth  Corporation
South Lakes Drive NC 28273-679
14001  Charlotte
Phone: (800) 739-7684