xxx 2011-02-08

New IndraLogic XLC PLC Family: Faster Automation Thanks to New Functions

New IndraLogic XLC PLC Family: Faster Automation Thanks to New Functions

IndraLogic XLC offers new functions, fast real-time communication via Sercos III, and is ideal for a variety of applications

(Charlotte, NC – ) Rexroth’s IndraLogic XLC PLC family enables scalable, controller-based and embedded PC solutions in conjunction with the company’s latest IndraControl device platform. Industrial PC-based hardware variants will round off the device portfolio in 2011.

Rexroth advanced the PLC programming using state-of-the-art PLC kernel, IndraLogic 2G, integrated homogeneously into the company’s IndraWorks software tool and the multitasking runtime system. This allows users to take advantage of many new functions for creating modular software projects in an end-to-end overall system in less time than before. Functions include convenient editor tools, object orientation as an extension to IEC 61131-3, and comprehensive function libraries as well as fast compilers for efficient generation of machine codes. The modular GATcompact (Generic Application Template) project template simplifies the process of designing new machines with enhanced software quality while reducing effort considerably.

End-to-end communication between the controller and decentralized system peripherals, such as inputs and outputs or drives, takes place via real-time Ethernet Sercos III. Fast PLC cycles to 250 µs enable optimum response times for handling time-critical process signals. IndraLogic XLC controllers come with versatile motion control functions, integrated into the run-time systems, to enhance the previous IndraLogic systems.

With its motion control functionality, the XLC handles machine applications ranging from simple point-to-point motion to the synchronization of multiple axes that use Rexroth’s FlexProfile to integrate complex motion sequences. The graphical profile editor in the Rexroth IndraWorks software tool offers numerous offline and online functions for this purpose. Master and slave interfaces for PROFINET RT, PROFIBUS and EtherNet/IP are also available, in addition to Sercos III, for integrating into a wide range of communication networks.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros in revenue in 2011.

To learn more, please visit

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innnovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit .

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at and .


Search press releases


Bosch Rexroth  Corporation
South Lakes Drive NC 28273-679
14001  Charlotte
Phone: (800) 739-7684