USA

Select your location

USA
 

Press

Content
2014-08-18

Bosch Rexroth maximizes manufacturing productivity with automation solutions for the machining industry at IMTS 2014

Booth visitors can learn about Sytronix variable-speed pump drives, which are for use in constant pr

Booth visitors can learn about Sytronix variable-speed pump drives, which are for use in constant pressure systems such as machine tools, offer energy savings.

Bosch Rexroth will exhibit a broad range of automation products and systems for improving productivity and energy efficiency, as well as safety and training in machine tool and CNC applications at IMTS 2014 in Chicago, IL, Booth E-5283, September 8-13, 2014.

The drive and control company will feature CNC platforms, advanced automation technologies and open programming tools to help optimize machining time and improve operational flexibility and precision production.

Booth highlights include:

Open Core Engineering Machining Demo

Visitors to the booth can participate in a demonstration that will show the flexible programming abilities of Bosch Rexroth’s Open Core Engineering system. Booth visitors can have their business card etched in metal on a specially-designed machine tool. Real-time machining visualization on a handheld tablet connected by wireless Ethernet demonstrates real-time machining monitoring, one example using the innovative Open Core Interface with the IndraMotion MTX CNC platform.

IndraMotion MTX CNC

IndraMotion MTX is a family of machine tool controls that provide open, scalable, CNC platforms for cutting, forming and machining applications. The newest platform version features the multi-core hardware CML 85, which supports 60 parallel NC-channels and control of up to 99 axes (up from 12 channels and 64 axes). In addition, the machine builder using IndraMotion MTX can now take advantage of simplified wiring of safety devices by using CIP Safety on Sercos (CSos) with the IndraDrive and PROFIsafe over Profibus DP.

IMS-I Integrated Measuring System for precise control of workpiece quality

The new IMS-I is an integrated measuring system incremental that combines highly rigid Rexroth Ball Rail and roller rail systems with an incremental length measuring system. It offers the measurement accuracy comparable to high-precision glass scales, making it ideally suited for use in external measuring systems on machine tools.

Safety on Board: Intelligent and Economical Machine Safety

Bosch Rexroth integrates safety into IndraDrive platforms so movement is monitored where it is generated, enabling extremely short reaction times and simpler safety architecture.

Bosch Rexroth offers three layers of integrated safety for its drive and controls products under Safety on Board:

  • Drive-based safety: The newest version of the safety-certified IndraDrive offers very fast response and up to 16 configurable safety modes (increased from 4 modes). The modes are configured in the IndraDrive based on mode selection; this can be done using either CIP Safety on Sercos (CSos), or via hard-wired safe zone modules.
  • Distributed PLC safety: Rexroth’s SafeLogic compact (SLc) is a small programmable safety PLC with support for up to 2 Sercos interfaces. A safety system with up to 16 axes can be configured between the SLc and IndraDrive devices, using a common Sercos Ethernet cable with minimal wiring.
  • Centralized PLC safety: Rexroth offers centralized safety PLC functionality with our IndraLogic XLC controller, IndraMotion MLC motion-logic platform and IndraMotion MTX CNC. Bus architectures supported include Sercos with CSos, which reduces wiring and safe motion programming time; in addition, PROFIsafe with Profibus DP is used for connecting safety I/O devices combined with normal Inline I/O.

Sytronix Variable-Speed Pump Drives for Machine Tools

The Sytronix FcP (frequency controlled pump drive) is an energy-efficient, variable-speed pump drive for use in constant pressure systems such as machine tools. It is available in the performance class 1.5-90 kW, and offers energy savings that range from 40% to 70%. In addition, the Sytronix FcP reduces average noise emission by up to 20 dB (A), has minimal or no cooling requirements and features a compact design to help save space.

Rexroth experts will also be available at IMTS 2014 to discuss a wide range of products including electrohydraulic controls and systems; linear motion components and modules; assembly and equipment for lean manufacturing; and electric drives, motors, controls and HMIs.

For more information about Rexroth’s involvement in CNC and machine tool automation, visit www.boschrexroth-us.com/imts .

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 36,700 associates generated sales revenue of approximately 5.7 billion euros ($7.6 billion) in 2013. To learn more, please visit www.boschrexroth-us.com

About Bosch:

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros ($61.2 billion). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its more than 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, Bosch applied for some 5,000 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, healthcare telemedicine and software solutions. For more information, please visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2015-01-26
Company News

Bosch Rexroth to exhibit latest automation and assembly technology at ATX West 2015

The Drive & Control Company will display its latest systems for automation and assembly productivity in booth 4400 at ATX West in Anaheim, February 10-12.


2014-10-24
Product News

Simply safe applications

The growth in use and complexity of automation across industries is driving a parallel growth in the complexity of human-machine interfaces (HMIs), resulting in an increased need for standardized, cost-effective functional safety for OEMs. To simplify the development of complex machines, Rexroth is integrating safety technology into the Sercos automation network.