USA

Select your location

USA
 

Press

Content
2014-09-11

Rexroth Offers New Series of Compact HMI Solutions – IndraControl VR Series

Bosch Rexroth IndraControl VR Series

With the new IndraControl VR Series of HMIs, Rexroth adds to their existing line of high-performance industrial PCs and HMIs.

The compact IndraControl VR series of embedded terminals complement the existing IndraControl V portfolio of larger screen HMIs and the PC-based panels, including the IndraControl VEP, VDP, VSP, and VPP series. The VR HMI uses a modern 16:9 format and is available in 4”, 7” and 9” sizes. The 7” and 9” panels also have a capacitive screen, multi-touch option. The multi-touch features provide the user familiarity of tablets and smart phones.

The IndraControl VR series of embedded terminals are a cost-saving alternative to the PC-based panels and utilize the Windows 7 Compact Embedded operating system. The ARM Cortex-A8 800 MHz processor provides excellent performance and reliability. 512 MB of RAM, 256 MB of flash memory as well as an integrated SD card memory slot ensure plenty of space for a robust application. Rexroth’s HMI programming software, WinStudio, can be used to develop applications for the VR controller, moving all Rexroth operator interfaces to the same programming development software.

Maximize your connectivity with a standard on-board Ethernet 10/100 Mbit port and 2 USB interfaces. There are +100 drivers available to connect the VR HMI to the controller of your choice. Small installation depths of 54 mm and IP65/20-protected displays make these HMIs very attractive to various industries.

For more information, visit www.boschrexroth-us.com/edc

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 36,700 associates generated sales revenue of approximately 5.7 billion euros ($7.6 billion) in 2013. To learn more, please visit www.boschrexroth-us.com

About Bosch:

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros ($61.2 billion). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its more than 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, Bosch applied for some 5,000 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, healthcare telemedicine and software solutions. For more information, please visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2015-12-03
Product News

Electromechanical cylinder from Rexroth: powerful with a hygienic design

Second generation with new design and an additional size


2015-10-26
Product News

Modular conveyor system for quick assembly

Quick planning, short-term commissioning, high conveying capacity: The VarioFlow plus chain conveyor system from Bosch Rexroth is optimized for quick assembly while combining particularly low-noise and economical operation. The choice of six conveyor widths between 65 and 320 mm, seven chain types and two models in aluminum and stainless steel with FDA-compliant materials opens up a wide spectrum of applications.