USA

Select your location

USA
 

Press

Content
2014-09-25

Intelligent software functions from Rexroth increase productivity and protect know-how

IndraMotion MTX

The Open Core Interface allows OEMs to realize individual functions and to seamlessly integrate devices such as smartphones and tablets into machine concepts.

Higher productivity through intelligent functions is an increasingly critical factor in the competitive ability of machine tools. Machinery manufacturers are therefore looking for ways to add new and unique functions while protecting their know-how at the same time. Open Core Engineering from Rexroth offers many such functional advancements with the CNC system solution IndraMotion MTX.

With Open Core Engineering, Rexroth enhances classic PLC programming by bridging the gap to IT automation. It increases engineering efficiency thanks to open standards, software tools, and function toolkits. Rexroth now offers machinery manufacturers the option of creating individual software functions independently, thereby allowing them to access the control via defined interfaces in real time. As a result, the Open Core Interface provides a new interface technology to Rexroth controls, allowing OEMs to develop individualized functional capabilities and set themselves apart from the competition. The Open Core Interface also enables seamless integration of smartphones and tablets into machine concepts, giving machine builders the ability to create useful mobile apps for numerous machine functions, such as allowing service technicians to perform wireless, remote machine diagnostics from anywhere.

To make it easy for machinery manufacturers to take advantage of the Open Core Interface, Rexroth has modeled the application know-how in software via predefined function toolkits. Machinery manufacturers need only provide the desired parameterization. For example, with the new IndraMotion MTX vcp function toolkit for volumetric error compensation, Rexroth's CNC automatically compensates for mechanical inaccuracies in the entire machining area. The three-dimensional compensation of deviations in position, straightness, rotation, and perpendicularity is especially useful in the case of large-volume components because errors outside of the margins can be costly. The necessary compensation values are recorded with a laser interferometer and saved in tables that the control system offsets in the process without performance losses. The bigger the machine workspace, the more significant the software function's correction effect. IndraMotion MTX vcp is able to improve volumetric accuracy in applications by over 90%.

The growing importance of software functions in machine tools carries with it an increased need to protect the machine builder’s proprietary knowledge. With the IndraMotion MTX encrypt function toolkit, machinery manufacturers and users alike now have a way to protect user programs from unauthorized third party access. Users can select and run encrypted programs on the machine; the program code is saved on the control exclusively in an unreadable format. It is also possible to bind the encryption to a specific piece of control hardware, so that encrypted programs can then run only on this one machine. The only requirement is to transfer the encrypted files to the machine. No interventions in parameters or software are necessary, giving machine users with a global production network an efficient way to protect their know-how.

In the field of machine safety, Rexroth offers additional options for increasing economic efficiency and uptime thanks to integrated safety technology. At the drive level, the safety-certified IndraDrive options S3/S4 now offer up to 16 modes using the CIP Safety on Sercos communication to the safety PLC over the Sercos automation bus Ethernet cable. For the distributed programmable safety PLC, the Safe Logic compact with CIP Safety on Sercos can provide the perfect solution. For centralized safety PLC within the CNC, the enhancement of the CNC system solution with a safety module for IndraMotion MTX is also available, using CIP Safety on Sercos to the IndraDrives and PROFIsafe on Profibus to the IO. Here the Open Core Engineering environment and the Safety PLC SafeLogic reduce programming time and effort, because process modifications have no feedback effects on the safety control. Machinery manufacturers can now achieve standardized safety from the control unit to the secure drive – all with minimal time and effort.

Finally, Rexroth meets user demands for greater energy efficiency with the IndraMotion MTX cta/ega software assistant, which is integrated into the control unit. It analyzes the duration and energy consumption of each machine movement. This database then lets programmers optimize motion control to increase energy efficiency while maintaining maximum productivity.

For more information: www.boschrexroth-us.com/oce .

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 36,700 associates generated sales revenue of approximately 5.7 billion euros ($7.6 billion) in 2013. To learn more, please visit www.boschrexroth-us.com

About Bosch:

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros ($61.2 billion). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its more than 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, Bosch applied for some 5,000 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, healthcare telemedicine and software solutions. For more information, please visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2015-10-23
Company News

Bosch Rexroth to exhibit latest assembly and handling technology at The ASSEMBLY Show 2015

The Drive & Control Company will display its latest systems for assembly flexibility and productivity in booth 419 at The ASSEMBLY Show in Rosemont, IL, October 27-29.


2015-03-26
Company News

Industry 4.0 Award for Bosch Rexroth Assembly Line

A new assembly line at Bosch Rexroth AG in Homburg/Saar, Germany, was recognized with the “Industry 4.0 Award” as a pioneer in the practical implementation of Industry 4.0. The prize was awarded by the trade journal Produktion along with ROI Management Consulting AG. The independent panel evaluated the assembly line, which was commissioned in the middle of 2014, to be the best implementation of Industry 4.0 in production.