Bosch Rexroth to exhibit hydraulics, drive and control technology for the plastics industry at NPE2015

Rexroth Sytronix variable-speed pump drive

The Sytronix variable-speed pump drive features a comprehensive selection of hydraulics-specific functionalities and is particularly suitable for use in exacting injection molding machines.

From electric and hydraulic drives and motors to conveyors and simulation systems, Bosch Rexroth will showcase technologies at NPE2015 that help plastics manufacturers operate with efficiency and precision through every step of the production process.

Bosch Rexroth will present multiple examples of drive and control, material handling technology and equipment for plastics manufacturing at the NPE2015 International Plastics Showcase. The company will be exhibiting in booth W4149 at the Orange County Convention Center in Orlando, FL, March 23-27.

Rexroth’s booth will feature leading-edge technologies including energy-saving Sytronix variable-speed pump drives, new Hägglunds hydraulic motors, and electrohydraulic controls. Additional technologies on display will include electromechanical cylinders and linear motion systems, simulation programs, the RexPak configurable hydraulic power unit and VarioFlow plus material handling conveyor systems. Applications engineers will be available throughout the show to discuss drive and control systems and equipment topics with attendees. Information on the popular Rexroth GoTo Focused Delivery program will also be available.

Key Rexroth highlights at NPE2015 include:

Sytronix SvP 7010 variable-speed pump drive

Sytronix drives combine the key advantages of both hydraulics and electronics. The variable-speed pump drives feature the reliability of powerful hydraulic systems with the energy efficiency of compact electronics. The SvP 7010 features a comprehensive selection of hydraulics-specific functionalities. Particularly suitable for use in exacting injection molding machines, the SvP 7010 increases dynamics and control accuracy with intelligent software functions while reducing energy requirements.

NEW Hägglunds CA 10 to 40 motor

Hägglunds motors feature high torque and power, a lightweight design and built-in overload protection. The new “beast” CA 10 to 40 series, to be unveiled at NPE, simultaneously delivers the highest power density, full torque and full speed. With a torque/weight ratio of 75 to 143 Nm/kg, the CA 10 to 40 offers a power density unmatched in the industry. For customers, the power density means energy and production efficiency. Compared to competitor solutions, CA 10 to 40 motors provide 10-15% more torque for the amount of energy put in. Further efficiency comes from the flexibility in the series, which includes four basic models and a wide variety of displacements. The Hägglunds CA 10 to 40 series is ideal for injection molding machines in the plastics industry, and additional applications are set to follow in the near future.

VarioFlow plus chain conveyor system

The VarioFlow plus chain conveyor system is a versatile, high-performance and standardized system ideal for achieving a fast time-to-market. With this modular and flexible chain conveyor system, users can easily configure individual, space-saving automation solutions for complex transportation tasks, even in particularly difficult environments.

GoTo focused delivery program

With Rexroth’s recently expanded GoTo Focused Delivery Program , customers can expect fast shipping on a broader range of items including electric drives and controls, hydraulics and linear motion products. The program offers industry-best delivery times and competitive pricing, delivering leading components to your doorstep.

Servo hydraulic axis

The servo hydraulic axis is a compact yet powerful tool combining electronic and hydraulic technologies. Like an electrical motor, it can be directly connected to a drive without tubes or a power unit. This electrohydraulic drive can also be installed directly onto the axis to save control cabinet space. For an even higher level of control precision, the servo hydraulic axis can be operated from a smart device.

Electromechanical cylinders

The electromechanical cylinder (EMC) is a completely modular system with an integrated ball screw assembly that is designed for high thrust/speed capability and greater flexibility and control. It can be used in applications that traditionally use hydraulic or pneumatic cylinders. Benefits include high energy efficiency, low environmental impact, no leakages, long service life, reduced downtime and high application flexibility. The EMC is part of Rexroth’s linear motion portfolio of products engineered to support higher speeds, higher load capacities and pinpoint precision.

For more information about Bosch Rexroth’s booth at NPE2015, visit .

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros ($7.6 billion) in 2013. To learn more, please visit

About Bosch:

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros ($61.2 billion.) (NB: Due to a change in accounting policies, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, the Bosch Group invested some 4.5 billion euros in research and development and applied for some 5,000 patents. This is an average of 20 patents per day. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at , and

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, healthcare telemedicine and software solutions. For more information, please visit , and


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670

Related Articles

Company News

Local supplier helps keep Bosch Rexroth orders error-free through kitting operation

To keep customer start-ups on track and to avoid assembly delays Bosch Rexroth Corporation, Bethlehem, PA, and Goodwill Keystone Area, Allentown, PA, team up to keep orders error-free.

Company News

Bosch Rexroth to exhibit latest assembly and handling technology at The ASSEMBLY Show 2015

The Drive & Control Company will display its latest systems for assembly flexibility and productivity in booth 419 at The ASSEMBLY Show in Rosemont, IL, October 27-29.