USA

Select your location

USA
 

Press

Content
2015-03-20

Bosch Rexroth variable-speed pump drive wins “Golden Mousetrap” best product award from Design News magazine

Sytronix SVP 7010

The Rexroth Sytronix SVP 7010 provides high dynamics and control accuracy along with energy efficiency and reduced noise level

Design News magazine, a leading mechanical and design engineering publication, named Rexroth’s Sytronix SVP 7010 variable-speed pump drive as a 2015 “Golden Mousetrap Best Product Winner” in the Automation and Control: Fluid Power Technologies category.

The magazine announced the winners of its annual awards program during a ceremony on February 10, 2015, at the Anaheim Marriott, in Anaheim, California, held in conjunction with the Pacific Design & Manufacturing trade show. The full list of winners is posted on the Design News website.

Golden Mousetrap Best Product awards were given in four major categories: Electronics and Test; Automation and Control; Design Tools; and Materials and Assembly. For more than 20 years, the Design News awards program has recognized exceptional products and celebrated engineering innovation.

This is the third time a Rexroth product has won a Golden Mousetrap award. Past winners were the A1VO35 variable displacement piston pump and IndraLogic XLC.

With Sytronix Variable Speed Pump Drives, including the new SVP 7010, Rexroth replaces the classic proportional valve technology with a drive system based on a motor pump unit that has high functionality and power density. Benefits include high dynamics, reduced noise and energy savings up to 80% as compared to conventional drive technologies.

The SVP 7010 is the latest innovation in the Sytronix family and can be used in both open and closed loop hydraulic circuits. Pumps for 2 or 4 quadrant operation are offered, with three levels of performance which allows the correct fit for nearly any machine configuration. Each Sytronix variable-speed pump drive consists of a unit equipped with frequency converter and control electronics, a standard or servo electric motor, and a hydraulic pump. SvP systems use the high dynamics of synchronous motors to achieve their considerable energy savings.

Overall, the Sytronix family comprises more than 100 preconfigured drive/pump combinations to meet the requirements of machine applications and performance. They are suitable for axis control tasks in both open and closed hydraulic circuits requiring high dynamics in addition to comprehensive electrical and electrohydraulic control options. Applications include plastics processing machines and presses.

For more information on Sytronix variable-speed pump drives, visit www.boschrexroth-us.com/sytronix

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros ($7.6 billion) in 2013. To learn more, please visit www.boschrexroth-us.com

About Bosch:

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros ($61.2 billion.) (NB: Due to a change in accounting policies, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, the Bosch Group invested some 4.5 billion euros in research and development and applied for some 5,000 patents. This is an average of 20 patents per day. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, healthcare telemedicine and software solutions. For more information, please visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2016-02-16
Corporate

Bosch Rexroth wins two “Golden Mousetrap” awards from Design News magazine for IndraDrive Mi and Hägglunds CA 10-40 motor

Design News magazine editors recognize Rexroth’s IndraDrive Mi for being cabinet-free and modular. Complete reallocation of all electric drive components to the machine saves production space. The second recognition goes to Rexroth’s Hägglunds CA 10-40 hydraulic motor for its extreme power density and high flexibility in lighter applications.


2015-08-06
Company News

Automation of measuring and testing machines in one step

National Instruments and Bosch Rexroth have introduced a perfectly matched control and drive solution at this year's NIWeek conference. The advantages of the control hardware CompactRIO and the programming environment LabVIEW are combined with dynamic servo technology. Rexroth’s pre-configured drive systems for measuring and testing machines cover a wide range of services and shorten the initial commissioning to just three minutes by means of a software wizard. Using a jointly tested and already proven interface, machinery manufacturers are programming motion sequences in the graphic environment LabVIEW without a single line of PLC code.