USA

Select your location

USA
 

Press

Content
2015-08-28

Bosch Rexroth to exhibit cabinet free technologies for the packaging industry at PACK EXPO 2015

Rexroth at PACK Expo 2015

Cabinet-free technologies from Bosch Rexroth open up valuable floor space and can help reduce wiring by up to 90%.

Demonstrations of cabinet-free technologies, motion and control products, along with in-depth working presentations of versatile conveyors, anti-slosh and anti-vibration systems will be shown at booth S-6127 at PACK EXPO 2015 in Las Vegas, September 28-30.

During PACK EXPO 2015, applications experts from Bosch Rexroth will exhibit the latest automation technology for next generation packaging machinery. These machines are cabinet-free, adaptive, efficient, and ready for Industry 4.0. Rexroth’s booth will highlight vibration-damping strategies, cabinet-free drive and power supply technology, flexible packaging conveyors, integrated safety and other solutions to help equip packaging machines for next generation requirements.

IndraDrive Mi cabinet-free drive technology: more production with less space

Rexroth’s IndraDrive Mi features maximum flexibility and efficiency for machine engineers and operators. Featuring cabinet-free drives and power supply, the solution saves space and energy. By eliminating drive electronics from the cabinet, a more compact controls enclosure can be mounted directly to the machine – freeing up valuable floor space and reducing wiring by up to 90 percent.

The newest generation features additional safety functions, extended communication options and intelligent control functions making it more useful and versatile than ever before.

Adaptive Systems: control movement for more productivity

Rexroth Adaptive Systems technology in the company’s IndraMotion MLD motion controllers provides the intelligence to apply vibration damping and avoidance control methods, which can increase throughput and extend machine life, in applications where sloshing, vibration and sway cause problems. Adaptive Systems technology can extend machine life, increase throughput by up to 50 percent and improve productivity by up to 40 percent.

VarioFlow plus: modular and flexible packaging conveyors

Rexroth’s VarioFlow plus offers a number of standardized options for a variety of application requirements with maximum interchangeability and modularity. To simplify selection and combination of the modules, Rexroth offers its MTpro planning software with Layout Designer . Users can design conveyors and even complex multi-conveyor and workstation systems, select components and output the results to CAD.

Additionally, valuable time can be saved during commissioning. The clever drive solution provides a great degree of planning freedom, and the motor mounting position can be chosen on-site. This reduces the selection of drive variants.

Electromechanical cylinder from Rexroth: powerful with a hygienic design

With the second generation EMC electromechanical cylinder , Rexroth expands the possibilities for utilizing compact drive units. With their hygienic design and IP65 protection class, they are now also suitable for applications with frequent cleaning cycles, such as those in the food industry. An optional force sensor allows decentralized process controls without a higher-level control system.

The available options in the newest generation allow for a long service life even when operated in demanding environments. The powerful EMC works extremely efficiently and economically at all times, making it a popular alternative to pneumatic linear drive systems.

During PACK EXPO 2015, engineers from Bosch Rexroth will also present Mechatronics @ Work, a demonstration platform created to showcase Rexroth drive and control technology and key mechatronics design and engineering principles.

As a leader in motion, drive and control solutions for the packaging and processing industries, Bosch Rexroth has pioneered innovative developments in mechatronics concepts and engineering approaches. The trade show exhibit -- which carries out functions like conveying, pick and place and robotic motion -- was created to showcase how effective mechatronics solutions utilize key principles such as energy efficiency, precision, modularity, ease of programming and operation, and intelligent integration.

The fully working system demonstrates functionality such as multi-axis motion, conveying and product transfer, advanced motion control and other automation tasks commonly required in applications such as case packing, collating and sortation.

For more information about the displays in Bosch Rexroth’s booth at Pack Expo visit www.boschrexroth-us.com

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 33,700 associates generated sales revenue of approximately $7.4 billion (5.6 billion euros) in 2014. To learn more, please visit www.boschrexroth-us.com

About Bosch:

Having established a regional presence in 1906 in North America, the Bosch Group employs some 28,700 associates in more than 100 locations, as of April 1, 2015. In 2014, Bosch generated consolidated sales of $11.3 billion in the U.S., Canada and Mexico. For more information, visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca .

The Bosch Group is a leading global supplier of technology and services. It employs roughly 360,000 associates worldwide (as per April 1, 2015). The company generated sales of $65 billion (49 billion euros) in 2014.* Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including its sales and service partners, Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic objective is to create solutions for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” Additional information is available online at www.bosch.com and www.bosch-press.com , http://twitter.com/BoschPresse .

*The sales figure disclosed for 2014 does not include the former joint ventures BSH Bosch und Siemens Hausgeräte GmbH (now BSH Hausgeräte GmbH) and ZF Lenksysteme GmbH (now Robert Bosch Automotive Steering GmbH), which have since been fully acquired.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2015-10-26
Product News

Modular conveyor system for quick assembly

Quick planning, short-term commissioning, high conveying capacity: The VarioFlow plus chain conveyor system from Bosch Rexroth is optimized for quick assembly while combining particularly low-noise and economical operation. The choice of six conveyor widths between 65 and 320 mm, seven chain types and two models in aluminum and stainless steel with FDA-compliant materials opens up a wide spectrum of applications.


2015-10-20
Product News

Ball rail systems: twice the service life and high travel accuracy

New BSHP ball runner block from Rexroth