Charlotte, NC, 2015-10-26

Modular conveyor system for quick assembly

Modular conveyor system for quick assembly

Optimized throughout for speed and efficiency: The VarioFlow plus modular chain conveyor system offers universal and quick application, easy planning and assembly. The system also boasts extremely qui

Quick planning, short-term commissioning, high conveying capacity: The VarioFlow plus chain conveyor system from Bosch Rexroth is optimized for quick assembly while combining particularly low-noise and economical operation. The choice of six conveyor widths between 65 and 320 mm, seven chain types and two models in aluminum and stainless steel with FDA-compliant materials opens up a wide spectrum of applications.

(Charlotte, NC – )Noise reduction is attracting increasing attention to continuously improve factory work environments. VarioFlow plus is one of Bosch Rexroth’s major contribution to noise reduction, with particularly low-noise operation thanks to sliding bars with lateral fixation, low-friction materials and patented hinge bolts. At the same time, VarioFlow plus provides optimum sliding properties for reduced wear, even with chain tensile forces up to 1,250 Newtons.

An example of VarioFlow plus’s flexible application can be found in the automotive industry: In order to improve handling and save space during transport, an innovative manufacturing cell based on VarioFlow plus is able to convey roof linings at a height of approx. three meters directly to a robotic unit at a processing station. Attaching and uncoupling the finished roof linings are the only manual procedures required in this fully automated solution. This results in increased productivity as factory personnel may use these time savings to complete other tasks. Currently, this automotive manufacturer operates four complete manufacturing lines using the same application of VarioFlow plus.

In combination with the innovative MTpro planning software, VarioFlow plus saves considerable time during project planning. The complete conveyor system can be designed in just a few steps – all the way from “drag and drop” selection of components to order placement, including verification of workpiece carriers and complete system configuration.

The advantages of VarioFlow plus continue once the system has been delivered. Start-up and commissioning are incredibly easy with this user-friendly modular system. Standardized components make the system exceptionally easy and fast to assemble, and ensure functionally safe operation.

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 33,700 associates generated sales revenue of approximately $7.4 billion (5.6 billion euros) in 2014. To learn more, please visit

About Bosch:

Having established a regional presence in 1906 in North America, the Bosch Group employs some 28,700 associates in more than 100 locations, as of April 1, 2015. In 2014, Bosch generated consolidated sales of $11.3 billion in the U.S., Canada and Mexico. For more information, visit , and .

The Bosch Group is a leading global supplier of technology and services. It employs roughly 360,000 associates worldwide (as per April 1, 2015). The company generated sales of $65 billion (49 billion euros) in 2014.* Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including its sales and service partners, Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic objective is to create solutions for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” Additional information is available online at and , .

*The sales figure disclosed for 2014 does not include the former joint ventures BSH Bosch und Siemens Hausgeräte GmbH (now BSH Hausgeräte GmbH) and ZF Lenksysteme GmbH (now Robert Bosch Automotive Steering GmbH), which have since been fully acquired.


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670

Related Articles

Product News

Ball rail systems: twice the service life and high travel accuracy

New BSHP ball runner block from Rexroth

Product News

Rexroth's North American GoTo™ Focused Delivery Program expands to over 4,000 materials, with improved lead times and increased order quantities

Over 400 product additions, shorter lead times and an updated app covering North America highlight Fall 2015 enhancements to Rexroth's popular fast delivery program.