USA

Select your location

USA
 

Press

Content
, 2015-12-03

Electromechanical cylinder from Rexroth: powerful with a hygienic design

EMC second generation

Without slots and recesses: second generation EMC electromechanical cylinder, with hygienic design

With the second generation EMC electromechanical cylinder, Rexroth expands the possibilities for utilizing these compact drive units. With their hygienic design and IP65 protection class, they are now suitable for applications with frequent cleaning cycles in the food industry. The new size EMC100-XC-2 increases the power density for feeding forces of up to 56 kN, e.g., for applications in forming technology. An optional force sensor allows decentralized process controls without a higher-level control system.

The axis penetrates the narrow working area and approaches different positions, or varies the pressing force: electromechanical cylinders combine the advantages of a slim cylinder with the possibilities provided by digital control of electrical drives. The ready-to-install drive units consist of anodized aluminum profiles in ISO standard dimensions, with an integrated ball screw drive. They cover variable-length strokes of up to 1,500 mm. In the newly developed second generation, Rexroth has implemented the principle of hygienic design in the cylinder body. There are no recesses or slots in which dirt can be trapped. The screws on the end face can be optionally sealed. Together with the version in IP65, which is also valid for the timing belt side drive, the EMC withstands frequent cleaning cycles and spray water.

For use in applications with particularly aggressive cleaning agents, the version in IP65 + R ensures a long service life with seals and scrapers made from chemically stable materials. A pressure compensation port prevents the occurrence of overpressure or negative pressure in the cylinder for the versions in IP65.

Additional size and optional force sensors

As the seventh size, the EMC100-XC-2 variant completes the product range. XC stands for extra capacity. The EMC-100-XC is longer than the EMC-100- NN-2, a larger axial bearing and larger ball screw drive provide up to 56 kN of feeding force—at the same profile cross section. This widens the usage for electromechanical cylinders from Rexroth towards more powerful applications in forming and machining.

Furthermore, Rexroth offers all sizes with an optional force measuring pin. This can be placed on the end of the piston rod as well as on the timing belt side drive. The sensors transmit the values with a +/- 10V analog signal to the drive. A Motion Logic System, which can be optionally integrated in the Rexroth drives, evaluates these signals and enables decentralized process control without a higher-level control system. The certified Safety on Board functions that are integrated in the drive simplify implementation of the Machinery Directive with low engineering effort.

In addition, the new housing is equal in its dimensions to those of the first generation. Interchangeability is thereby ensured. The technical data of the second generation is the same or better for all sizes, in comparison with the previous series. As a function of the piston rod position, the new EMC catalog now contains diagrams for the permitted radial piston rod force. With the newly designed lubrication points, users can integrate the electromechanical cylinder in central lubrication concepts. On request, the modules can be delivered by Rexroth without initial lubricant allowing users to apply industry-specific lubricants.

Rexroth provides a wide range of servomotors and drive controls which are suitable for the different sizes. Users can also operate the electromechanical cylinders using motors and controllers from other manufacturers. An online configurator supports selection of the suitable motor attachment kit.

Detailed information on the product can be found under www.boschrexroth.com/emc

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 33,700 associates generated sales revenue of approximately $7.4 billion (5.6 billion euros) in 2014. To learn more, please visit www.boschrexroth-us.com

About Bosch:

Having established a regional presence in 1906 in North America, the Bosch Group employs some 28,700 associates in more than 100 locations, as of April 1, 2015. In 2014, Bosch generated consolidated sales of $11.3 billion in the U.S., Canada and Mexico. For more information, visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca .

The Bosch Group is a leading global supplier of technology and services. It employs roughly 360,000 associates worldwide (as per April 1, 2015). The company generated sales of $65 billion (49 billion euros) in 2014.* Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including its sales and service partners, Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic objective is to create solutions for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” Additional information is available online at www.bosch.com and www.bosch-press.com , http://twitter.com/BoschPresse .

*The sales figure disclosed for 2014 does not include the former joint ventures BSH Bosch und Siemens Hausgeräte GmbH (now BSH Hausgeräte GmbH) and ZF Lenksysteme GmbH (now Robert Bosch Automotive Steering GmbH), which have since been fully acquired.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2014-10-24
Product News

Simply safe applications

The growth in use and complexity of automation across industries is driving a parallel growth in the complexity of human-machine interfaces (HMIs), resulting in an increased need for standardized, cost-effective functional safety for OEMs. To simplify the development of complex machines, Rexroth is integrating safety technology into the Sercos automation network.


2014-10-20
Product News

Rexroth’s North American GoTo Focused Delivery Program expands again, celebrating 5 years of fast deliveries

Nearly 300 product additions, shorter lead times, and a new GoTo Products app covering North America highlight Fall enhancements to Rexroth’s popular fast delivery program. 2014 also marks the GoTo Program’s 5th anniversary.