USA

Select your location

USA
 

Press

Content
, 2016-08-03

The right turn for higher energy efficiency

Bosch Rexroth EFC 3610/5610

EFC 3610 and EFC 5610 frequency converters from Rexroth.

All over the world, industrial end-users are demanding energy-efficient machines and equipment to significantly reduce operating cost and reduce their carbon footprint (CO2 emissions). By using demand oriented electromechanical energy, users are able to take vital steps in the right direction achieving those goals. Speed-controlled induction motors in variable speed pump drives for example can reduce electricity consumption by up to 80 percent in comparison to fixed-displacement drive applications. The EFC 3610 and EFC 5610 frequency converters from Rexroth address these potentials simply and economically. Scalable in performance and functionality features, the drives can be integrated into a wide range of automation environments with simple commissioning and open interfaces.

The intelligent frequency converters control speed as demanded, thus significantly reducing the energy consumption of pumps, compressors and fans. The frequency converters commonly known as variable frequency drives (VFD), AC drives or variable speed drives (VSD) can be integrated into many types of applications and machines as compact units for speed and torque control. Together with permanent magnet motors, the frequency converters increase energy efficiency while the adaptive pulse adjustment of the PWM frequency minimizes motor noise. Integrated energy counters measure actual consumption and capture valuable information for the energy usage optimization of machines and systems.

Commissioning without a PC

With the integrated control panel, commissioning can be done easily without external programming devices or a PC. From there, the user can start auto-tuning and enter, change or backup parameters. With switchover options between parameter sets and integrated PID control to increase flexibility as well as extensive connectivity options like Multi-Ethernet interface option (Sercos, EtherNet/IP, PROFINET, EtherCAT, and Modbus/TCP), designated fieldbus options (Profibus DP and CANopen) and additional I/O options, the devices are suitable for most machine applications.

The removable LED operator display panel shows all operating variables and has an integrated copy function. This accelerates the commissioning of several frequency converters with the same or similar parameter set and reduces the work required when exchanging equipment or in series production.

PC-based commissioning and diagnoses

The integrated mini-USB programming interface in conjunction with the free downloadable Rexroth IndraWorks Ds software tool, is used for easy commissioning via start-up wizard, monitoring and diagnoses or simple back-up, archive and restore parameters with any PC.

The drives have analog inputs and outputs, which can be configured as voltage or current interfaces. Digital inputs/outputs make simple direct coupling with a PLC possible. The assembly work required is significantly reduced by the integrated brake chopper and mains filter as well as time-saving installation technology using plug-in terminals and an attachment option on standard DIN rail.

Open interfaces for universal application

The EFC 3610 / 5610 frequency converters from Rexroth can be easily integrated into an automation network via Sercos, available through the optional Multi-Ethernet interface or other resident protocols like EtherNet/IP, PROFINET, EtherCAT, and Modbus/TCP. Modbus RTU interface is included as standard on the devices, other fieldbus options available are Profibus DP and CANopen. With the integrated sequence control with 16 levels, independent sequences can be parameterized. The protection function for pump operation and motor temperature monitoring protects the system during critical process conditions.

The new EFC3610 frequency converter series cover the power range from 0.4 to 22 kW or 0.5 to 30 hp, while the EFC5610 provides an expanded range up to 90 kW or 125 hp and safe torque off (STO). In addition to the freely definable V/f (V/Hz) operation, the EFC 5610 also offers vector control for an optimal torque curve. In heavy duty mode, the overload capacity can be maintained at up to 150 percent for 60 seconds. The high-torque EFC 5610 frequency converter also offers an optimal start torque of 200 percent at 0.5 Hz.


About Bosch Rexroth

About Bosch Rexroth

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31,100 associates generated sales revenue of approximately $5.99 billion (5.4 billion euros) in 2015. To learn more, please visit www.boschrexroth-us.com

About Bosch

Having established a regional presence in 1906 in North America, the Bosch Group employs some 28,700 associates in more than 100 locations, as of April 1, 2015. In 2014, Bosch generated consolidated sales of $11.3 billion in the U.S., Canada and Mexico. For more information, visitwww.boschrexroth-us.com , www.bosch.com.mx and www.bosch.ca .

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of $78.3 billion (70.6 billion euros) in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” Additional information is available online at www.bosch.com and www.bosch-press.com , http://twitter.com/BoschPresse .

<div style="text-align:center"># # #</div>

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2020-08-31
Corporate News

Changes to Bosch Rexroth management in North America

Greg Gumbs is to be appointed as the new President and CEO of Bosch Rexroth North America


2020-07-07
Product News

Aluminum Profiles for Personal Protective Devices from Bosch Rexroth

Made from modular aluminum framing, Rexroth’s protective devices can be used to help guard against airborne transmission of pathogens.