USA

Select your location

USA
 

Press

Content
, 2017-07-24

Bosch Rexroth’s EFC 5610 frequency converter now enhanced with Safe Torque Off over the entire power range

Bosch Rexroth EFC 5610

The EFC 5610 frequency converter with Safety on Board (STO – Safe Torque Off)

The upgraded EFC 5610 with STO safety by Bosch Rexroth offers up to Cat. 4/PLe, SIL3 safety levels for safety relevant appliactions now over the complete power range. Safe Torque Off (STO) is a function used to prevent unexpected motor movement while connected to power during an emergency situation. Scalable in performance and functionality features, the EFC 5610 can be integrated into a wide range of automation environments with simple commissioning and open interfaces.

The newly enhanced EFC 5610 frequency converter (VFD) now provides STO functionality from 0.4 kW (0.5 hp) to 90 kW (125 hp). In addition to the advanced safety options, the EFC 5610 offers vector control for an optimal torque curve. The vector control can be easily parameterized and chosen over the standard U/f technology mode. Parameterization can be done through the operator display panel or via free downloadable IndraWorks Ds software tool by use of a PC connected via USB cable to the engineering port of the EFC.

In heavy duty mode, the overload capacity can be maintained at up to 150 percent for 60 seconds. The high-torque EFC 5610 frequency converter also offers an optimal start torque of 200 percent at 0.5 Hz. From 5.5 kW (7.5 hp) devices can optionally be parameterized for Normal Duty mode (ND), providing higher continuous power levels at 120 percent overload.

Using an option module, the EFC 5610 can be extended by a Multi-Ethernet interface with Sercos, EtherNet/IP, PROFINET, EtherCAT and Modbus/TCP or fieldbus interfaces such as PROFIBUS or CANopen and can be integrated into all common automation solutions.

With the Multi-Ethernet interface and the OpenCore interface (OCI for Drives), the EFC 5610 is prepared for modern machine concepts in the environment for Industry 4.0. With available libraries, the EFC 5610 can be controlled via most programming languages.

The EFC 5610 furthermore offers flexible expandability with application-specific functionalities, such as Rexroth Sytronix - variable speed pump drive technology (electro/hydraulic multi-technology).

With the improved safety features of the EFC 5610 frequency converter, Rexroth offers an economical and safety-conscious solution for a variety of applications in which valuable energy has to be used responsibly. Marked with the Rexroth 4EE systematic approach, Rexroth continues its commitment to energy efficiency without compromising on the quality.

For more information about Rexroth’s EFC 5610, please visit www.boschrexroth-us.com/efcx610 .

About Bosch Rexroth

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31,100 associates generated sales revenue of approximately $5.99 billion (5.4 billion euros) in 2015. To learn more, please visit www.boschrexroth.com .

About Bosch

Having established a regional presence in 1906 in North America, the Bosch Group employs some 32,500 associates in more than 100 locations, as of December 31, 2016. According to preliminary figures, in 2016 Bosch generated consolidated sales of $13.7 billion in the U.S., Canada and Mexico. For more information, visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca .

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). According to preliminary figures, the company generated sales of 73.1 billion euros ($80.9 billion) in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 450 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

# # #

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2020-03-25
Product News

Bosch Rexroth launches new load sensing valves

The RM10 and RM15 are easy to configure, compact, general purpose, multi-application valves fit for use in today’s mobile machines


2020-03-17
Product News

Bosch Rexroth Launches Piston-Gear Pump Assembly with Common Suction Port

New tandem pump configuration simplifies design and installation of combined axial/gear pump systems to save space on mobile machines