USA

Select your location

USA
 

Press

Content
, 2017-08-03

Bosch Rexroth introduces DRn 5020 to Sytronix product family

Bosch Rexroth Sytronix

Ideal for retrofits, DRn 5020 is a versatile, energy-efficient solution for constant pressure systems. Easy add-on to existing DR systems using an EFC5610 pump controller and pressure transducer.

The DRn 5020 is the newest addition to the Sytronix line-up. The Sytronix DRn 5020 is an easy and powerful solution for a constant pressure pump control providing noise reduction, energy savings and increased system efficiencies. Advanced displacement management optimizes the performance during partial load and idle operation.

The Sytronix DRn 5020 is a powerful, cost-effective solution for hydraulic power units (HPU) with small to high power requirements. Specifically designed for constant pressure systems, the DRn 5020 provides higher performance for presses, metallurgy, wood working or central hydraulic systems. The motor-pump consists of an industry standard pressure compensated variable displacement pump, an induction motor and Rexroth’s pump control EFC 5610 enhanced with Sytronix DRn 5020 application functionality.

The EFC 5610 pump control used in the DRn 5020 system is available from 4 kW (5 hp) to 90kW (125 hp).

The DRn 5020 system distinguishes itself with high response time due to the fast-acting pump, even with a traditional low-dynamic induction motor. The pump control optimizes the operating speed, maximizing efficiency and minimizing noise produced by these constant pressure systems

The system supports standalone operation or Multi-Ethernet communication options, providing flexibility for integration into a variety of system topologies.

DRn systems are well suited for OEM applications or retrofit of existing systems. They provide efficient solutions using industry standard pumps and motors, providing the added benefits of low-noise, reduced energy consumption and longer component lifetimes.

For more information about Rexroth’s Sytronix product group, please visit https://www.boschrexroth.com/en/us/products/systems-and-modules/sytronix-variable-speed-pump-drives/index

About Bosch Rexroth

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31,100 associates generated sales revenue of approximately $5.99 billion (5.4 billion euros) in 2015. To learn more, please visit www.boschrexroth.com .

About Bosch

Having established a regional presence in 1906 in North America, the Bosch Group employs some 32,500 associates in more than 100 locations, as of December 31, 2016. According to preliminary figures, in 2016 Bosch generated consolidated sales of $13.7 billion in the U.S., Canada and Mexico. For more information, visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca .

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). According to preliminary figures, the company generated sales of 73.1 billion euros ($80.9 billion) in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 450 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

# # #

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2020-08-31
Corporate News

Changes to Bosch Rexroth management in North America

Greg Gumbs is to be appointed as the new President and CEO of Bosch Rexroth North America


2020-07-07
Product News

Aluminum Profiles for Personal Protective Devices from Bosch Rexroth

Made from modular aluminum framing, Rexroth’s protective devices can be used to help guard against airborne transmission of pathogens.