Press

Content
, 2017-12-14

Motors for intelligent drives

IndraDyn S

Intelligent, powerful and flexible: The new MS2N servo motors are now also available with an integrated encoder in SIL3 PLe

High-dynamic, precise and easy to configure – the latest developments in the motor spectrum from Bosch Rexroth follow these basic requirements for automation and electrification. Thanks to their high dynamics and force density, they enable the shortest cycle times in many applications. The high-torque synchronous servo motor, MS2N, is also available with an integrated encoder in the SIL3 PLe category for demanding tasks with SafeMotion. Also, in conjunction with IndraDrive control units, the MS2N motors can be used as a data source for I4.0.

Rexroth offers the IndraDyn S series MS2N in six sizes with up to five lengths each. The series covers the power range from 4 Nm to 360 Nm maximum torque and 0.8 Nm to 215 Nm continuous torque at standstill. Machine manufacturers can choose from three encoder systems, all finely graded in both precision and resolution. For the electrical connection of power and encoder signal, Rexroth provides an innovative single cable connection, as well as conventional two-cable solutions with highly flexible cable options and practical quick-lock.

Thanks to the new motor construction and an optimized electromagnetic design, this new generation is able to achieve significantly reduced torque ripple. This is especially important for maintaining constant path velocity and increased product quality. In addition, the developers at Bosch Rexroth have reached up to 30 percent higher torque density. The motors are significantly more compact despite their enhanced performance. Therefore, machine manufacturers can use smaller motors in existing drive tasks or use more power within a given motor compartment. Up to five times overload capacity guarantees the fastest acceleration and optimum dynamism for all sizes. With different degrees of rotor inertia, machine manufacturers can offer application-oriented design for different masses on the axes.

Due to high-quality materials, the MS2N motors achieve significantly greater continuous power, even at higher speeds. Also, thanks to their optimized winding technology, the motors help to reduce internal losses. Plus, the new generation accomplishes dramatic increases in energy efficiency.

The high-torque synchronous servo motor MS2N has proven itself in the Bosch Rexroth Connected Automation range with their high dynamic, synchronization and a robust single-cable connection, with up to 75 m cable length.

The servo motor is also available with an integrated SafeMotion encoder from the high-performance SIL 3, PL e safety class. This eliminates the need for additional safety components in the system. The motor model in the IndraSize engineering tool enables safe, quick and simple drive configurations that correspond exactly to real operation.

In the new IndraDyn S series MS2N, intelligence now reaches all the way up to the motor. Individual measurements of each individual motor, as well as saturation and temperature data, are stored in the respective motor's memory and are automatically processed by IndraDrive controllers. This information greatly increases the precision of the torque and reduces the tolerance range to a fraction of previously accepted values. Also, for the first time, the servo motor provides data as well. This feature allows OEM’s to implement Industry 4.0 applications, such as condition monitoring and predictive maintenance, economically and without additional components.

About Bosch Rexroth

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros ($5.5 billion) in 2016.

To learn more, please visit www.boschrexroth-us.com

About Bosch

Having established a regional presence in 1906 in North America, the Bosch Group employs nearly 32,800 associates in more than 100 locations, as of December 31, 2016. In 2016 Bosch generated consolidated sales of $13.7 billion in the U.S., Canada and Mexico. For more information, visit www.boschusa.com, www.bosch.com.mx and www.bosch.ca.

The Bosch Group is a leading global supplier of technology and services. The company employs roughly 390,000 associates worldwide (as of December 31, 2016) and generated sales of 73.1 billion euros ($80.9 billion) in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at www.bosch.com, www.bosch-press.com, http://twitter.com/BoschPresse.

# # #

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com



Related Articles

2018-01-15
Corporate

Connect with Bosch Rexroth’s latest automation innovations at ATX West 2018

The Drive and Control Company will demonstrate its latest advancements in Connected Automation at ATX West 2018 in Anaheim, CA February 6-8, 2018


2018-01-10
Corporate

Bosch Rexroth MoveWithRexroth.com Microsite Offers the Latest Hydraulics Innovations

Rexroth’s microsite now features the latest product innovations for both Factory Automation and Hydraulics & Heavy Industry