Nexo offers a direct measuring system for accurate torque and angle detection.
Combining economical operation and safety critical tightening capability, Bosch Rexroth’s Nexo nutrunner can handle the most demanding applications and is suitable for both large and small scale production. Its decentralized intelligence is located directly onboard the tool which enables operation without cable connections or the need for an external controller. By integrating the control of the tightening process, the highest level of reliability is possible - even in wireless dead zones.
The Nexo is durable enough to handle demanding applications such as safety critical use within the automotive industry, yet still accurate enough to safely fulfill sensitive battery cell production. Furthermore, the device’s intelligent design can utilize product variables such as a serial number to determine which unique tightening process/recipe to execute based on the model or product variant.
Users also benefit from simple integration into their existing WiFi network, enabling an easy wireless transfer of tightening results to their servers. The cordless design provides an easy to use, ergonomic solution with a high degree of mobility for use in areas where traditional cabled or air technology is not possible. The integrated high-quality digital sensors for torque and angle provide excellent accuracy, repeatability, durability, and process documenation – no external sensors or hardware required.
Nexo now offers up to 100 Nm maximum torque and a max speed of 880 rpm. All versions are available with a browser-based operating system and an optional barcode scanner. All Nexo are capable of class A tightening (safety critical) in accordance with VDI/VDE2862 and supports both 2.4 and 5 GHz WIFI networks.
For more information, visit here. .
About Bosch Rexroth
Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros ($5.5 billion) in 2016.
To learn more, please visit www.boschrexroth-us.com
About Bosch
Having established a regional presence in 1906 in North America, the Bosch Group employs nearly 32,800 associates in more than 100 locations, as of December 31, 2016. In 2016 Bosch generated consolidated sales of $13.7 billion in the U.S., Canada and Mexico. For more information, visit www.boschusa.com, www.bosch.com.mx and www.bosch.ca.
The Bosch Group is a leading global supplier of technology and services. The company employs roughly 390,000 associates worldwide (as of December 31, 2016) and generated sales of 73.1 billion euros ($80.9 billion) in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.
Additional information is available online at www.bosch.com, www.bosch-press.com, http://twitter.com/BoschPresse.
# # #
Susan Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com
Explore Rexroth’s connected automation, assembly, and handling solutions in booth #4400 at ATX West 2019, February 5-7, in Anaheim, California
Rexroth’s handheld CC-ErgoSpin product line enables a higher degree of process reliability and longer work times with minimal fatigue.