USA

Select your location

USA
 

Press

Content
, 2018-04-26

Bosch Rexroth offers digitalization of analog interfaces in hydraulics via IO-Link

IO Link

Lower connection costs for components thanks to an M12 connector and electronic name plate. (Copyright: Bosch Rexroth AG)

Reduced connection costs and increased uptime: Rexroth harnesses the benefits of the IO-Link open standard for hydraulic actuators and sensors. Our popular 4WRPEH proportional control valves and HEDE10 pressure switches are now available with IO-Link interfaces via a decentralized, fast IO-Link Master IP67 I/O system, S67E. That means that users now have direct access to all data provided by the actuator/sensor in addition to the field bus.

Industry 4.0 is often much closer than we think: While individual suppliers offer proprietary solutions for networking of machine peripherals and better utilization of data, there are established and open standards that do exactly the same thing. IO-Link is supported by approximately 150 companies and enables digital communication of peripherals with control in parallel to common field buses. With proportional valves and pressure switches, Bosch Rexroth now offers the first hydraulic actuators and sensors with these networking capabilities. By adding IO-Link capabilities to these products, Rexroth continues to promote the integration of fluid technology into Industry 4.0 applications since IO-Link enables vertical connection of components all the way into IT systems.

IO-Link standardizes and simplifies wiring thanks to standard M12 connectors with unshielded 3-conductor/5-conductor cables, eliminating any need for time-consuming and mistake-inducing individual hand wiring Project planning can be performed using the engineering tool of the respective PLC manufacturer. All modules needed for communication are available for free with the IoT-ready PLC systems ILC, as well as Motion Control systems. In combination with IndraWorks Engineering, they enable direct access to project planning, parameterization and testing. The parameters can always be adapted to any new operating conditions.

The standardized electronic name plate of these plug & play devices reduces machine and system downtime. Remote access by authorized maintenance personnel allows them to call up and evaluate operating conditions such as temperature, operating hours and error status during running production as part of a predictive maintenance concept. Wear and system errors can be predicted before failure occurs and causes machine downtime, with any devices needing servicing located and displayed. Thanks to IO-Link, no specialized training is needed to replace devices: Components are clearly identified via site ID and an electronic name plate for easy replacement using interchangeable components. Parameterization is carried out automatically by the IO-Link Master without any need for additional action by the technician. As a result, replacement of components can be completed successfully without causing any additional problems.

Following the 4WRPEH proportional valve and the HEDE10 pressure switch, Bosch Rexroth intends to outfit additional hydraulic actuators and sensors with IO-Link interfaces to continually round out the product range.

About Bosch Rexroth

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros ($5.5 billion) in 2016.

To learn more, please visit www.boschrexroth-us.com

About Bosch

Having established a regional presence in 1906 in North America, the Bosch Group employs nearly 32,800 associates in more than 100 locations, as of December 31, 2016. In 2016 Bosch generated consolidated sales of $13.7 billion in the U.S., Canada and Mexico. For more information, visit www.boschusa.com, www.bosch.com.mx and www.bosch.ca.

The Bosch Group is a leading global supplier of technology and services. The company employs roughly 390,000 associates worldwide (as of December 31, 2016) and generated sales of 73.1 billion euros ($80.9 billion) in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at www.bosch.com, www.bosch-press.com, http://twitter.com/BoschPresse.

# # #

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2019-01-22
Corporate

Experience the latest in connected automation and IoT with Bosch Rexroth at ATX West 2019

Explore Rexroth’s connected automation, assembly, and handling solutions in booth #4400 at ATX West 2019, February 5-7, in Anaheim, California


2019-01-15
Corporate

Safely assemble with confidence using Bosch Rexroth's ErgoSpin

Rexroth’s handheld CC-ErgoSpin product line enables a higher degree of process reliability and longer work times with minimal fatigue.