The IoT Gateway Rack is ready to plug into any standard 110V outlet.
The IoT Gateway Rack is an IP65-rated enclosure containing Rexroth’s award-winning IoT Gateway. Additionally, it includes all the necessary wiring and connections to connect PLCs, I/O and other data sources for collection, processing and forwarding of plant floor data to upper-level data systems.
CE rated and UL listed, the IoT Gateway Rack is one of the latest additions to Rexroth’s automation portfolio. This IP65-rated system neatly contains all the necessary components, including Rexroth’s IoT Gateway, to connect data sources to upper-level data systems. Rexroth’s IoT Gateway technology is a configured, not programmed, solution, meaning it doesn’t require knowledge of specific programming languages and makes it easy to get up and running. Additionally, it’s powered by industry-standard 110V outlets so no additional, expensive wiring is required to power the Rack.
The IoT Gateway Rack has the ability to collect legacy PLCs and simple digital and analog I/O to collect data from machines that were manufactured without Industry 4.0 data transfer capabilities, making it the ideal solution for retrofitting older machines. It’s Plug-and-Play design allows Original Equipment Manufacturers to use the IoT Gateway Rack as an optional addition to their existing machines. This allows them to easily provide Industry 4.0 capabilities for customers who require the additional functionality without changing the main design of the machine.
Additional highlights of the IoT Gateway Rack include:
• Contains three Ethernet ports, one HDMI port, one USB port with Wi-Fi and 4G options for full connectivity capabilities
• Works with popular data streams for data collection and communication such as OPC UA, OPC DA, TCP/IP, MQTT and REST
• Connects to standard databases such as MySQL and MongoDB
• Rated for industrial environments
• Connects to popular PLC systems and I/O, as well as well-known cloud architecture
See the IoT Gateway Rack in action in booth #S-1654 at PACK EXPO 2018.
About Bosch Rexroth
As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, more than 30,500 associates generated sales revenue of approximately 5.5 billion euros ($6.2 billion) in 2017.
To learn more, please visit www.boschrexroth-us.com
About Bosch
Having established a regional presence in 1906 in North America, the Bosch Group employs nearly 34,500 associates in more than 100 locations, as of December 31, 2017. In 2017 Bosch generated consolidated sales of $13.7 billion in the U.S., Canada and Mexico. For more information, visit twitter.com/boschusa, twitter.com/boschmexico and www.bosch.ca.
The Bosch Group is a leading global supplier of technology and services. It employs roughly 402,000 associates worldwide (as of December 31, 2017). The company generated sales of 78.1 billion euros ($88.2 billion) in 2017. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 125 locations across the globe, Bosch employs some 64,500 associates in research and development.
Additional information is available online at www.bosch.com, www.iot.bosch.com, www.bosch-press.com, www.twitter.com/BoschPresse.
Exchange rate: 1 EUR = $1.12968
# # #
Susan Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com
See the Factory of the Future at work in booth #4400 at ATX West 2019, February 5-7
Explore Rexroth’s connected automation, assembly, and handling solutions in booth #4400 at ATX West 2019, February 5-7, in Anaheim, California