USA

Select your location

USA
 

Press

Content
2014-01-14

Rexroth to highlight latest advances in hydraulics technology at CONEXPO 2014

Rexroth to highlight latest advances in hydraulics technology at CONEXPO 2014

The innovative A1VO axial piston pump is just one of many hydraulic products Bosch Rexroth is featuring at CONEXPO to help customers improve productivity and boost energy efficiency.

Company emphasizes technology to boost energy efficiency, improve productivity, and expand capabilities of mobile machinery


Bosch Rexroth exhibits the newest developments in hydraulics technology, including Axial Piston Variable Pumps, Mobile Controls, High-Torque Hydraulic Motors, Drive Train solutions, and more in booth 80216 at the CONEXPO-CON/AGG show, March 4-8 in Las Vegas.


Visitors to the Rexroth booth can expect to see a broad range of leading hydraulics technology used in loaders, cranes, telehandlers, excavators and other mobile equipment. The company will display several notable products and systems designed to boost energy efficiency, improve productivity, and expand capabilities of mobile machinery.


Axial piston variable pumps

The A1VO axial piston pump is designed specifically for the smaller power classes of mobile machinery and offers reduced fuel consumption, optimized power efficiency and a compact design. In addition to these benefits, the A1VO offers an economical switch from open-center design to a load-sensing system. The series is now available in two displacement sizes: 18 and 35 cm3.


The A24VG axial piston variable double pump offers a higher pressure level for greater power density and good efficiency for hydrostatic drives in closed circuit applications. It features a compact design for tight installation conditions in equipment such as wheel loaders, skid loaders and all-wheel drive vehicles.


Mobile controls

Rexroth offers a range of mobile controls products that includes all hydraulic function elements necessary for direction, pressure, flow and check functions. Visitors to the booth will learn about the company’s M4 Rapid Production Program (RPP) which is intended to provide quick delivery for standard assemblies in custom arrangements and flexibility to fit most applications while allowing for field adjustments where possible.


High-torque hydraulic motors

The Hägglunds CBM motor is the world’s latest and largest low-speed high-torque radial piston cam curve design hydraulic motor. It is 50 percent lighter than its predecessor while offering more efficiency with higher power and speed capability. The Hägglunds CBM motor opens up many new applications with its versatile mounting and improved performance and is supported by many existing Rexroth service centers in North America, including the company’s new service center in Houston.


Also on display is Rexroth’s Rineer high-torque vane motor, a medium-speed high-torque hydraulic motor that uses a patented vane crossing vane design. It is available with through-hole and bearing boxes for direct-drilling applications. The company‘s recent Fountain Inn, SC, facility expansion has added manufacturing capacity for the Rineer high-torque vane motor to significantly lower product delivery time.


Drive train solutions

The Shift on Fly (SoF) , and 2+1 hydrostatic drive systems offer new possibilities for the travel drive on telehandlers, municipal vehicles and fast-moving wheel loaders in the compact class. The SoF is a hydrostatic drive with a two-stage axle gear box, while the 2+1 is a hydrostatic drive with two parallel hydraulic motors driving an axle gear box. Key benefits include a continuously variable transmission ratio, reverse capability under full load, faster response and maneuverability, and high performance and traction at low engine speed.


The Rexroth High-Efficiency Traction control system (HET) will also be on display as a simple solution for automated all-wheel drive activation on compact vehicles with hydrostatic wheel motors. HET eliminates the need for electronics or sensors and offers high efficiency for high speed and continuous traction on critical terrain.


Additional offerings

Other technology on display includes new transmission units, mobile electronics, compact hydraulics, product selection software, control valves, and radial piston motors. In addition, attendees will learn about Bosch Rexroth’s new hydraulics manufacturing and engineering facility expansion at Fountain Inn, SC, and new service center in Houston, TX, which will help strengthen the company’s contribution to the construction and mobile equipment markets across the Americas.


Visit Bosch Rexroth at CONEXPO in South Hall 3, booth 80216.

For more information go to www.boschrexroth.com/conexpo.


About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros in 2012. To learn more, please visit www.boschrexroth-us.com


About Bosch:

The Bosch Group is a leading global supplier of technology and services. In fiscal 2012, its roughly 306,000 associates generated sales of 52.5 billion euros. Since the beginning of 2013, its operations have been divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.8 billion euros for research and development in 2012, and applied for nearly 4,800 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at www.bosch.com and www.bosch-press.com

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com




Related Articles

2019-04-25
Corporate

Rexroth’s MoveWithRexroth.com microsite relaunched with refreshed design and content

The microsite’s new design showcases Bosch Rexroth’s new branding and offers viewers an improved user experience


2019-04-23
Corporate

Bosch Rexroth to exhibit the latest technologies for marine and offshore industries at OTC 2019

Using interactive demos such as the Rally Simulator, Bosch Rexroth will display its advancements for the offshore sector at OTC 2019 in Houston, Texas