1. Home
  2. Company
  3. Press Portal
Small Handling Belt (SHB) and Small Handling Lead Screw (SHL)
Small Handling Belt (SHB) and Small Handling Lead Screw (SHL)
Press release

The new economical linear modules for lighter loads

The new Small Handling Belt (SHB) and Small Handling Lead Screw (SHL) from Bosch Rexroth offers low operating costs and less downtime for a variety of applications.

SHB

  • Load capacity of up to 110 lbs centered
  • Max. speed of 3 m/s
  • Stroke lengths from 100 mm to 2,000 mm in 50 mm increments

SHL

  • Load capacity of up to 6 lbs centered
  • Max. speed of 0.06 m/s
  • Stroke lengths from 25, 50, 100, 150, and 200 mm

Bosch Rexroth is now offering linear modules for small handling applications, the SHB and SHL. These modules are suitable for more than factory automation. They are designed for lighter load applications such as in medical labs, universities, and vision systems. With simple USB to laptop connectivity, monitoring and controlling has never been easier.

The new SHL lead screw driven module is designed for light load, low cost applications. Made with a 55 mm wide aluminum frame, the SHL is precise and compact. This module comes with the option of motor and controller or just the motor, depending on the requirements. The SHL is perfect for college projects, industrial automation, biomedical applications, and so much more.

The new SHB belt driven linear module is compact, yet robust. It offers stroke lengths up to 2 meters and load capacities up to 110 lbs centered. The SHB measures at 40 mm wide and boasts a repeatability of < 20 microns. This module also comes with the option of motor and controller or just the module, depending on the requirements.

Simplified Ordering

Both the SHL and SHB modules are available with I/O, E-stop ports, and cables (-C versions). To make it simple, there are only two configuration choices to choose from: the stroke and whether I/O and E-stop ports are required. All the product specifications, stock levels, and ordering will be available on the Rexroth Store website, making these linear modules accessible for everyone.

Small Handling Belt (SHB) and Small Handling Lead Screw (SHL)

Basic Information Bosch Rexroth

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, more than 29,600 associates generated sales revenue of around 5.2 billion euros in 2020.

Basic Information Bosch

The Bosch Group is a leading global supplier of technology and services. It employs roughly 402,600 associates worldwide (as of December 31, 2021). The company generated sales of 78.7 billion euros in 2021. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT provider, Bosch offers innovative solutions for smart homes, Industry 4.0, and connected mobility. Bosch is pursuing a vision of mobility that is sustainable, safe, and exciting. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to facilitate connected living with products and solutions that either contain artificial intelligence (AI) or have been developed or manufactured with its help. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. With its more than 400 locations worldwide, the Bosch Group has been carbon neutral since the first quarter of 2020. The basis for the company’s future growth is its innovative strength. At 128 locations across the globe, Bosch employs some 76,100 associates in research and development, of which more than 38,000 are software engineers.

Press Contact

Please get in touch with our Press Contact

Related News

Linear Motion Technology

10/06/2025

Durable cylinders for high forces: High power electromechanical cylinders cover heavy-duty applications with forces up to 250 kN

Bosch Rexroth is expanding the electromechanical cylinders in the EMC-HP high-power series

Read More
Linear Motion Technology

21/05/2025

Bosch Rexroth introduces pre-parameterized stepper motors for single and multi-axis systems

Solutions for handling small parts must be compact, cost-effective, and quick to implement.

Read More
Company
Assembly Technology
Linear Motion Technology
Electric Drives and Controls

15/01/2025

Bosch Rexroth to Demonstrate Innovative Linear Motion Technology for Automating Medical and Packaging Applications

Demonstrations and booth presentations covering multiple Bosch Rexroth automation capabilities for medical and packaging will be featured at MD&M West 2025.

Read More