PI 036-14 Lohr am Main, 2014-04-28

Expanded All-Rounder Now More Efficient and Flexible

Energy-efficient motors enable environmentally-friendly production with the Rexroth TS 2plus transfer system. In addition, the new modular units increase flexibility.

The Rexroth TS 2plus transfer system with new energy-efficient motors and modular units

  • Optimized motors save energy
  • New modular units make way for further applications

Overall efficiency is a key topic when it comes to investments in assembly systems, demonstrated by low energy consumption and high flexibility. Systems designed for ever increasing market requirements not only have to cope with changing batch sizes and shorter product cycles, but also meet demanding environmental objectives. Rexroth now offers energy-efficient motors for its TS 2plus transfer system, as well as additional modular units for even more application options.

Ever shorter innovation and product cycles are decisive factors when selecting transfer systems. At the same time, environmental aspects are becoming increasingly important when looking at overall efficiency. Bosch Rexroth is facing up to these challenges and has countered them by expanding its TS 2plus transfer system with new modular units.

An effective use of energy is the main feature of the new Rexroth motors for all TS 2plus modular units. The 3-phase motors already meet the future requirements of efficiency class IE3, save around 15% energy, and pay off within a maximum of two years. In addition to continuous operation and connection to variable-speed frequency converters, the new motors also enable start-stop operation. This saves even more energy, as the transfer section only runs as needed. The Rexroth for Energy Efficiency (4EE) concept makes a major contribution to ensure that operation of the TS 2plus transfer system is cost-effective and energy-efficient. The 3-phase motors are certified in accordance with CE, cURus, and CCC, and work with common global voltages so that they can be implemented in all major industrial countries.

Additional modular units make the Rexroth transfer system even more flexible and versatile. The new lift transverse unit can transfer work piece pallets sized 240 x 240 up to 640 x 640 mm and with an overall weight of up to 130 kg from longitudinal to transverse sections. The conveyor medium is a robust, quiet duplex chain which has proven itself in harsh ambient conditions. Integrating the lift gate into the standard offering has made the previous special solution even more cost-effective. The lift gate supports belt sections and can be folded up effortlessly via gas pressure springs. As a result, the user has easy access to the transfer system for maintenance. The new lift rotate unit lifts work piece pallets up to 240 kg from the conveyor system and rotates them by 90° or 180° so that the products are transferred to the processing stations in the correct position.

The versatile Rexroth TS 2plus transfer system is reliable even under challenging conditions, such as in ESD environments or in clean room and dry room applications, and is thus suitable for a variety of sectors, from the automotive industry, to electronics and electrical technology, through to medical technology and the optical industry.

Bosch Rexroth at Automatica 2014 in Munich – hall A6, booth 502

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, its roughly 281,000 associates generated sales of 46.4 billion euros in 2013 (Note: due to a change in the legal rules governing consolidation, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its more than 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, Bosch applied for some 5,000 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at , and


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573

Related Articles

Press Information

The next generation of Linear Modules: fit for one-point lubrication and challenging applications

The third generation of MKK and MKR Linear Modules from Rexroth provides a considerably expanded range of equipment options for the familiar space-saving dimensions of the previous series. The ready-to-install linear axes are ready to be connected to the one-point lubrication systems. In the corrosion resistant versions, hard chrome plated ball screw drives and ball rails ensure a high resistance to chemicals.

Press Information

Digital engineering in Linear Motion Technology: Rexroth is expanding its range of eTools

What do the configuration of a Linear Motion System and online shopping have in common? In the case of Bosch Rexroth, the answer is easy: Thanks to numerous intuitive eTools, selecting, dimensioning and ordering components and systems for Linear Motion Technology is just as easy and convenient as shopping online in general. Because while you used to have to trawl through parts catalogues and look up the right material numbers, the majority of this is now done by online configurators and engineering tools. In order that machine and system designers can also benefit from more efficient workflows in the future, Rexroth is constantly redeveloping its range of digital tools and ensures new functions and even better handling with its updates.