International
 

Press

Content
PI 065-14 Lohr am Main, 2014-08-05

99 drives, 60 channels, one CNC controller

CNC system solution IndraMotion MTX advanced: particularly suited to rotary transfer machines with up to 99 axes.

IndraMotion MTX from Rexroth – now even more powerful

and easier in engineering

In the new software version 14 VRS, the multi-core CNC system solution IndraMotion MTX advanced now supports the control of up to 99 axes in 60 channels with only one CNC controller. Open standards, software tools and function packages increase the engineering efficiency – even with complex machines. With Open Core Engineering, Rexroth also combines the previously seperate machine tool and IT worlds and allows machine manufacturers to configure customized software functions.

Production of increasingly complex geometries with lower tolerances in less time: productivity is a very important criterion for machine tool end users; however it is not the only one. Factors such as energy efficiency, machine safety, ease of use and integration into the IT world are getting more important. To stand out from the competition, machine manufacturers look for ways to differentiate themselves through independent software functions and provide the end user with additional benefits. Rexroth incorporated these requirements with the latest version of the IndraMotion MTX CNC system solution.

In the most powerful variant, IndraMotion MTX advanced, the CNC system now controls up to 99 axes. The controller can execute tasks in parallel in up to 60 channels. Even with the maximum number of axes, the multi-core processor CNC guarantees high performance and short cycle times. Thus, IndraMotion MTX is suitable, for instance, for complex rotary transfer machines with numerous workstations. The increased performance of the controller also reduces the system costs because additional hardware that was previously required is saved.

Open Core Engineering from Rexroth increases efficiency for the machine manufacturer throughout the entire engineering process. Software tools and function packages automate routine tasks. They replace time-consuming programming with simple parameterization for numerous tasks. Consistent use of open, cross-vendor standards make it a future proof system solution. In addition to PLC automation, Open Core Engineering creates a bridge to the IT world.

New degrees of freedom for individual software functions

This opens up new degrees of freedom for machine manufacturers to independently create individual software functions in high-level programming languages. These functions access the controller in real time via the interface technology of Open Core Interface. This technology is currently offered only by Rexroth and enables rapid networking of machines in industry 4.0 concepts. In addition, Open Core Interface allows for the seamless integration of smart phones and tablets in machine concepts to simplify operation. With application programs, otherwise known as "Apps", for these smart devices, service technicians can quickly perform diagnostics for the machines wirelessly and from anywhere.

Safety – from controllers to drives

In the area of machine safety, Rexroth offers additional ways to increase efficiency and availability. Extending the CNC system solution by adding the safety PLC SafeLogic and the "Safety Manager" function toolkit from the Open Core Engineering environment, reduces the time and effort involved in configuration and startup.

Changes in the process have no effect on the safety control. Thanks to the certified Safety on Board safety features integrated in the servo drives, the machine manufacturers can implement standardized safety measures with minimum time and effort.

Rexroth 4EE increases energy efficiency

Rexroth supports the user demand for higher energy efficiency with the software package IndraMotion MTX Efficiency Workbench. Machine manufacturers use it to analyze the duration and energy consumption of each machine movement. With the help of this database, you can optimize motion control with your CNC programming. This increases both the energy efficiency and productivity. Furthermore, Rexroth helps machine manufacturers take advantage of full the potential to increase energy efficiency. For this, the industry specialists use the universal Rexroth 4EE system. It combines an energy-efficient system design with optimized component efficiency as well as demand-oriented performance and energy recovery.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros. (NB: Due to a change in accounting policies, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, the Bosch Group invested some 4.5 billion euros in research and development and applied for some 5,000 patents. This is an average of 20 patents per day. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2016-08-11
Press Information

The five most expensive savings ideas for the maintenance of machinery and equipment

Machine downtime is always expensive, especially if a whole production line comes to a standstill as a result. For new machinery, the machine manufacturer is still liable, but afterwards the responsibility for maintenance lies solely with the user. Maintenance staff must constantly justify their "unproductive" costs and, hence, try to reduce them. However, some short-term saving ideas lead to nothing but higher total costs in the end. The following are the five most expensive, and unfortunately, not uncommon errors when it comes to machine maintenance.


2018-09-18
Press Information

Mikron Multistar CX-24: Flexible for large-scale production

With the Multistar CX-24, Mikron Machining combines the productivity of a rotary transfer machine with high flexibility for smaller batch sizes. For this, Mikron relies on the open CNC system MTX from Rexroth. The completely redesigned transfer system comprises 24 stations and can be equipped with up to 20 CNC axis. This allows users to quickly and flexibly convert the Multistar CX-24 to different variants within a part family.