International
 

Press

Content
PI 069-14 Lohr am Main, 2014-09-17

Hydraulic Motion Control - intelligent hydraulics ready for networking

The digital axis control HMC from Rexroth

The Hydraulic Motion Control (HMC) from Rexroth: open, simple, and flexible

Automation experts all agree: in increasingly networked production environments to Industry 4.0, centralized intelligent axes are the future. Provided they can communicate via open interfaces with higher-level systems. The new Hydraulic Motion Control HMC from Rexroth meets this essential requirement. The future-proof 1-axis controller for hydraulic drives with multi-Ethernet and multi-encoder interfaces as well as PLC programming in accordance with IEC 61131-3 dovetails a wide variety of concepts.

Open communications interfaces and a migration from hydraulic functions into the software are the key prerequisites for decentralized intelligence. The new, drive-based Motion Logic System HMC from Rexroth meets these requirements with open interfaces and the best-in-class hydraulic controller.

Increasingly more machine manufacturers are using real-time Ethernet protocols for coordinated motions. Yet this is a decision they are not always free to make. Big end customers are more frequently specifying a preferred protocol in order to standardize the communication architecture. OEMs must therefore equip their series in parallel with different Ethernet variants. The HMC from Rexroth decidedly reduces the costs involved. The HMC's multi-Ethernet interface supports all standard protocols on one single piece of hardware: the automation bus Sercos, Ethernet/IP, PROFINET RT as well as EtherCAT and PROFIBUS. The HMC merges an IEC 61131-3-compliant programming language with a powerful motion control for hydraulic drives. As slave, it takes over the decentralized control of an axis where it decouples the hydraulics from the automation process.

The best-in-class hydraulic controller incorporates decades of application experience in the field of hydraulic axis control, which is depicted in ready-to-use software. The software automatically offsets the special characteristics of fluid technology. The pre-defined hydraulic functionalities encompass closed-loop position, pressure, force, and velocity control, alternating control, and open-loop controlled operation. IndraWorks software supports the commissioning, parameterization, and diagnosis of the HMC.

The HMC from Rexroth opens up new networking possibilities. With the decentralized intelligence and the multi-Ethernet interface, users can easily integrate the physical advantages of hydraulics, such as high power density and simple wear-free overload protection into modern, future-proof machine concepts.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros. (NB: Due to a change in accounting policies, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, the Bosch Group invested some 4.5 billion euros in research and development and applied for some 5,000 patents. This is an average of 20 patents per day. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2020-02-25
Press Information

Safety, efficiency and beyond

Compact, gearless and modular: Hägglunds hydraulic direct drive systems from Bosch Rexroth provide high flexibility in rubber manufacturing. Physical and digital innovations, together with service expertise, are creating further possibilities to keep rubber customers ahead.


2019-11-21
Press Information

5 facts about hydraulics that may surprise automators

It is often the case that younger designers and engineers have hardly had any experience of hydraulics as part of their training. They are primarily concerned with software and think along digital lines. They are only really interested in the movements and the resulting data. Drive physics is what makes the difference in many cases here. Hydraulics come into their own whenever large forces and robustness are required, however many young designers are not very familiar with this technology. Here are some facts showing why the use of modern, connected hydraulics is easier and more cost-effective than many of them realize.