Press

Content
PI 002-15 Lohr am Main, 2015-01-18

Electromechanical cylinder from Rexroth: powerful with a hygienic design

Without slots and recesses: second generation EMC electromechanical cylinder, with hygienic design

Second generation with new design and an additional size

With the second generation EMC electromechanical cylinder, Rexroth expands the possibilities for utilizing these compact drive units. With their hygienic design and IP56 protection class, they are now also suitable for applications with frequent cleaning cycles, such as those in the food industry. Furthermore, the new size EMC100-XC-2 increases the power density for feeding forces of up to 56 kN, e.g. for applications in forming technology. An optional force sensor allows decentralized process controls without a higher-level control system.

The axis penetrates the narrow working area and approaches different positions, or varies the pressing force: electromechanical cylinders combine the advantages of a slim cylinder with the possibilities provided by digital control of electrical drives. The ready-to-install drive units consist of anodized aluminum profiles in ISO standard dimensions, with an integrated ball screw drive. They cover variable-length strokes of up to 1,500 mm. In the newly-developed second generation, Rexroth has implemented the principle of hygienic design in the cylinder body. There are no recesses or slots in which dirt can be trapped. The screws on the end face can be optionally sealed. Together with the version in IP65, which is also valid for the timing belt side drive, the EMC withstands frequent cleaning cycles and spray water.

For use in applications with particularly aggressive cleaning agents, the version in IP65 + R ensures a long service life with seals and scrapers made from chemically stable materials. A pressure compensation port prevents the occurrence of overpressure or negative pressure in the cylinder for the versions in IP65.

Additional size and optional force sensors

As the seventh size, the EMC100-XC-2 variant completes the product range. XC stands for extra capacity. The EMC-100-XC is longer as the EMC-100-NN-2, a larger axial bearing and larger ball screw drive provide up to 56 kN of feeding force - at the same profile cross section. This widens the usage for electromechanical cylinders from Rexroth towards more powerful applications in forming and machining.

Furthermore, Rexroth offers all sizes with an optional force measuring pin. This can be placed on the end of the piston rod as well as on the timing belt side drive. The sensors transmit the values with a +/- 10V analog signal to the drive. A Motion Logic System, which can be optionally integrated in the Rexroth drives, evaluates these signals and enables decentralized process control without a higher-level control system. Furthermore, the certified Safety on Board safety functions that are integrated in the drive simplify proper implementation of the Machinery Directive with low engineering effort.

The new housing is equal in its dimensions to those of the first generation. Interchangeability is thereby ensured. The technical data of the second generation is the same or better for all sizes, in comparison with the previous series. As a function of the piston rod position, the new EMC catalog contains now diagrams for the permitted radial piston rod force. With the newly designed lubrication points, users can integrate the electromechanical cylinder in central lubrication concepts. On request, the modules can be delivered by Rexroth without initial lubricant. In this way, users can apply industry-specific lubricants directly.

Rexroth provides a wide range of servomotors and drive controls which are suitable for the different sizes. Users can also operate the electromechanical cylinders using motors and controllers from other manufacturers. An online configurator supports selection of the suitable motor attachment kit.

Detailed information on the product can be found under www.boschrexroth.com/emc

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros. (NB: Due to a change in accounting policies, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, the Bosch Group invested some 4.5 billion euros in research and development and applied for some 5,000 patents. This is an average of 20 patents per day. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com, www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.