024-12 Lohr, 2012-05-07

Automatic All-Wheel Drive

Automatic All-Wheel Drive

For instance road sweepers benefit from High Efficiency Traction Control as energy efficient single-wheel drive with automatic all-wheel drive activation.

New single-wheel drive solution from Rexroth switches automatically and at just the right moment between 2-wheel and all-wheel drive.

  • All-wheel drive only when needed – automatically activated
  • HET valve block for high energy efficiency
  • Compact plug-and-play solution for simple vehicle integration

The greatest possible traction in difficult conditions while retaining optimal energy efficiency – often conflicting goals when developing or purchasing single-wheel driven municipal vehicles and work machines. Bosch Rexroth now introduces their HET High Efficiency Traction Control, a new hydrostatic drive solution that combines and meets both requirements.

The energy efficiency of HET is based among other things in the fact that all-wheel drive is only activated when needed – fully automatically with no driver intervention. If in difficult terrain for example a wheel loses its grip with the ground, slip rapidly increases. The Rexroth MCR radial piston motor driving the wheel responds by increasing the oil flow. The rising oil flow causes a momentary and seamless transmission of the torque to the series-connected MCR motor and wheel located on the other axle. By using this “slip activation” of the all-wheel drive the High Efficiency Traction Control provides reliable response to the terrain and saves significant energy compared with fulltime all-wheel drive.

In less difficult terrain or on the road the wheels in the driving axle generally have sufficient traction. The radial piston motors on the other axle then simply “free-run.” Only the two permanently driven MCR motors transfer the power from the diesel engine. However, slip occurs not only when a wheel spins. Due to deformation of the rubber tires it is actually always present to a greater or lesser degree. Even this comparatively slight slip will also result in an increasing oil flow by the driven radial piston motors. The increased flow is hydraulically clamped between the driving and free-running radial piston motor, resulting in a significant loss of efficiency for the entire travel drive.

HET completely eliminates this efficiency loss. A specially developed valve block ensures that “excess” hydraulic oil caused by natural slip is directed to the low-pressure side of the circuit.

In addition, the HET valve block is not located in the main oil flow, thereby minimizing losses even further. Integration of the purge function and other design features make the unit highly compact, while the plug-and-play solution reduces time and money associated with installation and piping.

The HET uses no sensors or control electronics. In addition to the newly developed valve block it consists of proven standard components from Rexroth such as the A4VG or A10VG pump as well as MCR motors with constant or selectable displacement volume. This makes the HET a flexible solution for use in a wide variety of vehicle types such as municipal vehicles, mini-dumpers or small front loaders. It is designed to cover the greatest possible number of requirements, including vehicle speed or installation space.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue in 2010.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Additional information can be accessed at,


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573