136-11 Lohr, 2011-12-09

Systematic pneumatics competence

Complete pneumatic control cabinet

Complete pneumatic control cabinet

Ready-to-install, complete pneumatics systems allow machine and system manufacturers to concentrate fully on their core business without the need to develop each and every drive concept themselves. Rexroth takes on a complete package of customer tasks, including planning, configuration, and assembly of pneumatic control panels, control cabinets, or handling systems. These are tested thoroughly and then shipped ready-to-install. The company also supplies customer-specific product adaptations or special solutions for cylinder/valve combinations.

Rexroth can come up with a custom solution that is derived from its extensive range of modular products for every application. As a result, specially configured actuators are provided with the right valve technology, required accessories, and appropriate compressed air preparation, before being thoroughly tested and delivered ready for installation. Modular system solutions or customer-specific designs also easily fulfill special application specifications related to installation space, speed, or hygienic design.

Rexroth also modifies standard pneumatic components and comes up with special solutions for various industries. For example, thanks to a multi-position cylinder that was developed in conjunction with Rexroth, a customer can implement up to 13 different settings with just one actuator.

Customers who would like to order the entire pneumatics system for a machine can benefit from another service offered by Rexroth. The “pneumatics set” concept lets customers order all the pneumatics components required for a machine or system. Delivery of a tested set with just one material number simplifies many of the customer’s internal processes, such as ordering, incoming goods checks and quality control, and logistics, and also provides additional security.

The pneumatics sets are put together by the respective sales contact, who directly compiles a parts list with a total price. The order is checked again at the Rexroth logistics center before the set's price is confirmed and a material number generated for the specific configuration. The set is then delivered directly from the central warehouse to anywhere the customer may be.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue in 2010.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros in fiscal 2010. For 2011, the company forecasts sales of more than50 billion euros and a headcount of a good 300,000 by the end of the year. The Bosch Group comprises Robert Bosch GmbH and its more than350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Additional information can be accessed at ,


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573