PI 004-15 Lohr am Main, 2015-02-04

With virtual commissioning your goals are achieved faster

Virtual Commissioning with Open Core Engineering reduces engineering time and cut the costs and risks for machinery manufacturers.

Integrated engineering of roll-to-roll machines with Open Core Engineering

Flexible electronics is about to break through to mass production, and many machine manufacturers are currently working on new machine concepts for it. Virtual Commissioning significantly reduces the development time of economical but complex control technology for roll-to-roll processing. In turn, this helps a machine manufacturer reduce the costs and risks during commissioning. With Open Core Engineering, Rexroth opens up new possibilities to implement a comprehensive range of simulation programs.

In conventional machine manufacturing the commissioning of the machine control is one of the last steps before delivery is made to the customer. If problems occur here that require rectifying with later design changes, then the costs rise exponentially, and the time schedules come under enormous pressure.

Commissioning using simulation software offers new opportunities for rapid control prototyping, minimizing these risks, and reducing engineering time. It allows machine manufacturers to commission the machine control in parallel, or even prior to the hardware installation. Open Core Engineering from Rexroth is a pre-requisite in achieving these goals. The integrated interface technology within the Open Core Interface can be used for in various virtual development environments created simulations for virtual commissioning. Machine operators use the simulation on a virtual machine, before successfully tested programs are transmitted to the real machine. Hence they shorten the time-to-market.

The simulation program and the Rexroth control directly exchange all the necessary data and commands for virtual commissioning via standard Ethernet and without additional PLC code. The controller adapts to the simulation speed.

The simulations on the PC allow the economic optimization of PLC programs. Decentralized control tasks are embedded seamlessly into the intelligent servo technology by allowing the simulations high-level programming language direct access to drive parameters. Thus, manufacturers of for example OLED roll-to-roll machines use virtual commissioning to adjust the pre-defined multi-zone web tension controller from Rexroth to their concepts, or to program movements in the workspace. They can safely simulate errors and take appropriate countermeasures.

In Addition to the open standards Modelica and FMI, Rexroth supports the established tools MATLAB / Simulink and LabVIEW.

Other practical options for integrated engineering with Open Core Engineering for automation will be shown by Rexroth during the LOPEC 2015 on the booth B0 308, and in a machine module of dr. Schwab GmbH on the demo Line 2015 (B0 307). During the fair, this production line consisting of machines and modules from different vendors produces electroluminescent films the size of a business card.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, its roughly 290,000 associates generated sales of 48.9 billion euros in 2014. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its more than 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic goal is to deliver innovations for connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at , and


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573

Related Articles

Press Information

The five most expensive savings ideas for the maintenance of machinery and equipment

Machine downtime is always expensive, especially if a whole production line comes to a standstill as a result. For new machinery, the machine manufacturer is still liable, but afterwards the responsibility for maintenance lies solely with the user. Maintenance staff must constantly justify their "unproductive" costs and, hence, try to reduce them. However, some short-term saving ideas lead to nothing but higher total costs in the end. The following are the five most expensive, and unfortunately, not uncommon errors when it comes to machine maintenance.


The factory of the future creates added value through flexibility and agility

In future production environments demands on adaptability will rise. This development can only be realized by separating hardware and software in automation. Bosch Rexroth AG promotes this development primarily with a broad product spectrum from sensors to drive and control technology to software solutions.