Press

Content
100-11 Lohr, 2011-09-21

Straightforward changeover to electrohydraulics

Rexroth's TVC

Rexroth's TVC is a package solution ready for immediate use. Tractor manufacturers thus save time and money developing their own expensive software solution.

Tractor Valve Control (TVC) from Rexroth makes the control and operation of electrohydraulic valves easy

  • No software development costs for tractor manufacturers
  • Straightforward installation with a plug-in package
  • Functionality in accordance with practical requirements

The high efficiency of modern tractors is based above all on intelligent electronics. The related expense encountered by tractor manufacturers for the development of electronics and software is however substantial. With Tractor Valve Control (TVC), Rexroth is now presenting a ready-to-use software package that allows manufacturers to simply and cost-efficiently integrate electrically controlled valves into their systems. TVC is supplied as a ready-to-use, easily installed plug-&-play solution, including the controller. It assumes the job of reliably controlling electro-hydraulic valves and can be used in tractors with fixed and variable pumps.

TVC can control up to six electro-hydraulic auxiliary directional valves such as the SB23 and SB33 EHS1. Tractor manufacturers can quickly and easily integrate the standard package into their hydraulic concept without having to invest time in their own development. The advanced software thus makes it easier, especially for smaller manufacturers, to change over to using electro-hydraulic valves, with the related benefits for the end user. The practical and intuitive TVC operating philosophy allows the oil flow through the directional valves to be precisely adjusted and limited. TVC's convenient operation and sensitive control thus makes the job of the tractor driver much easier.

The optimum TVC software version is determined by the number of valves employed and by the type of pump. The parameter settings are made beforehand at the production plant. Further functions such as electro-hydraulic hitch control and gearbox functions can be integrated on request, reducing installation complexity, installation space and costs even further.

Rexroth at Agritechnica 2011: Hall 09 - Stand E17

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue in 2010.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Additional information can be accessed at www.bosch.com ,www.bosch-press.com

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de