International
 

Press

Content
PI 006-15 Lohr am Main, 2015-03-04

Intelligent hydraulic power units: Networkable and energy-efficient

The ABPAC series is prepared for Industry 4.0

New ABPAC series from Rexroth makes hydraulics ready for open data exchange

The new hydraulic power unit series ABPAC from Rexroth fully reflects electrification and Industry 4.0. Being provided with decentralized intelligence and optional sensor packages, the power units continuously acquire all operational states and communicate via open interfaces with higher control levels or authorized smartphones and tablet PCs. Variable-speed pump drives Sytronix cut energy consumption by up to 80 percent.

Configuring online, exchanging data via open interfaces, sensing operational states continuously: In networked automation of the future, hydraulics feature the same intelligence and communication capability as electric drives. In the new hydraulic power unit series ABPAC Rexroth already turned this requirement into reality.

Thanks to the interface technology of Open Core Engineering the power units fit seamlessly and future-proof into horizontally and vertically networked production environments. An integrated, universally usable sensor package continuingly acquires all relevant system states of the power unit: Degree of clogging of filters, oil quality, sensors for working, suction and accumulator pressure, oil level and various temperatures. ABPAC makes sensor data, system variables and derived status messages available to standardized interfaces. The user can read these messages out over the Ethernet bus either via the machine control or an integrated web browser – wireless from a smartphone or a tablet PC.

Energy-efficient drive technology

All power units are designed for the use of variable-speed pump drives Sytronix FcP. They reduce the speed in partial load operation in line with demand and cut the energy requirement of hydraulics by up to 80 percent. Moreover, it is also possible to integrate drives of the Sytronix SvP family, in which the special requirements of fluid power technology are already taken into account in the software of these intelligent drives. The commissioning and diagnosis tools for them are identical to those for electric axes from Rexroth.

With tank capacities of 100 to 400 liters, the ABPAC series meets the requirements of all common hydraulic applications. The hydraulic basic functions are already integrated in a multi-function block. It features additionally an interface to further, standardized hydraulic control assemblies. Users can compose their desired power unit online on the basis of the world’s greatest hydraulics and electrohydraulics program for industrial applications. The online tool guides the user on the basis of technical key data and suggests suitable assemblies. Directly after the configuration is completed, the program provides a complete documentation package.

ABPAC are suitable for the entire spectrum of applications of hydraulics in stationary machines, from cutting machine tools and woodworking through to presses or plastics machinery.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, its roughly 290,000 associates generated sales of 48.9 billion euros in 2014. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its more than 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic goal is to deliver innovations for connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2020-02-25
Press Information

Safety, efficiency and beyond

Compact, gearless and modular: Hägglunds hydraulic direct drive systems from Bosch Rexroth provide high flexibility in rubber manufacturing. Physical and digital innovations, together with service expertise, are creating further possibilities to keep rubber customers ahead.


2019-11-21
Press Information

5 facts about hydraulics that may surprise automators

It is often the case that younger designers and engineers have hardly had any experience of hydraulics as part of their training. They are primarily concerned with software and think along digital lines. They are only really interested in the movements and the resulting data. Drive physics is what makes the difference in many cases here. Hydraulics come into their own whenever large forces and robustness are required, however many young designers are not very familiar with this technology. Here are some facts showing why the use of modern, connected hydraulics is easier and more cost-effective than many of them realize.