022-12 Lohr, 2012-03-22

Energy-efficient hydraulic easily integrated

Pump and motor are optimally aligned

Only if pump and motor are optimally aligned and if the software can read the movement task with all characteristics of the fluid technology, the power consumption can be reduced at the same performan

Bosch Rexroth makes integration easier with ready-to-install kits

Besides its productivity, the energy consumption of a machine becomes increasingly the criterion of the purchase decision. Therefore, already during production, manufacturers must keep an eye on the energy efficiency of the individual components. A drive concept with variable speed pump drives promises a high potential of savings. To keep the engineering effort as low as possible, the machine manufacturer expects unproblematic implementation in its machine concept. When choosing Sytronix Variable Speed Pumps from Rexroth, the integration will be an easy and safe experience.

Machines must solve various motion tasks, and there are just as many approaches to solve them. Design engineers want to change to energy saving hydraulics but without having to pay high costs for selection, design, programming, and commissioning. The outstanding technical competence of Bosch Rexroth allows the development of an integrated solution from one source: the Sytronix family, where Rexroth combined its hydraulic pumps and electric drives. The manufacturer’s hydraulic knowledge is already implemented in the best-in-class controls. This provides many advantages: the design engineer can integrate the ready-to-install, pre-configured solutions very easily and quickly in his engineering environment without having to deal with the details of programming.

When choosing Sytronix kits that are designed for the respective motion task, Rexroth’s industry experts provide advice. For instance the 14 kits of the FcP 5000 series are in particular suitable for simple hydraulic tasks, such as clamping or gripping. In these economic solutions, frequency converters with internal gear pumps handle the demand-depending power generation. For more sophisticated tasks in plastic machinery or forming technology, designers can choose among 47 pre-configured kits of the SvP 7000 series. These kits cover a wide range of applications in five performance classes with various servo-motors and pump types. More than 80 kits of the product series DFEn 5000 are particularly suitable for axis control tasks in the high power range. The intelligent pump is only offered by Rexroth, and it controls the swivelling angle and the motor speed and is suited for the four quadrant operation.

Users reduce power consumption of the hydraulics by up to 80 percent with Sytronix while being able to keep the same productivity. Apart from that, they reduce the medium noise emission by up to 20 dB (A) and increase the lifetime of the hydraulic medium through lower heat input.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue in 2010.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Additional information can be accessed at ,


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573