Press

Content
PI 020-15 Lohr am Main, 2015-04-11

Intelligent self-sufficient systems for powerful drive tasks

Stand-alone self-contained electro-hydraulic servo axis (SHA): Functionalities identical to that of electromechanical variants.

Stand-alone self-contained electro-hydraulic servo axis (SHA) from the Rexroth portfolio are fully compatible with electromechanical variants

Stand-alone axes from Rexroth with identical servo-drives for actuators with mechanical or hydraulic force transmission offer new degrees of freedom for machine manufacturers in finding drive solutions that suit specific application requirements. The versions with hydraulic transmission are provided with their own, decentralized fluid circuit. The installation, commissioning and connection to controls and Industry 4.0 environments via a Multi-Ethernet interface or ProfiBus are identical on both variants.

Stand-alone self-contained electro-hydraulic servo axis from Rexroth largely consist of electrical and hydraulic series components. They pair all the functions known from servo-drives with the physical advantages of fluid power technology such as high power density and robustness. The standardized sub-assemblies, that is, hydraulic cylinder, control block and motor/pump group, form the basis for these linear axes of modular design. They are fitted with their own, closed fluid circuit and do without a central hydraulic power unit. The leak-free fluid circuit requires only a very small amount of hydraulic fluid. Rexroth delivers the axes completely pre-assembled, filled with hydraulic fluid and commissioned. The system is virtually maintenance-free and the fluid medium service life corresponds to that of the axis.

Identical commissioning

In all of the stand-alone axes from Rexroth, servo-drives of the IndraDrive family within a power spectrum of up to 630 kW are used. Thanks to their decentralized intelligence and standardized software, the type of force transmission is irrelevant for the higher-level control. Also when it comes to commissioning, there is no difference. A power connection and a communication connection to the higher-level control are sufficient. For this, IndraDrive controllers with their Multi-Ethernet interface support all common Ethernet protocols like Sercos, ProfiNet, EtherNet/IP, EtherCAT, Powerlink or ProfiBus.

Intelligent, reliable and energy-efficient

The software of the IndraDrive servo-drives assumes the control of the linear unit. The SHA library contained in the software automatically takes account of all specialties of fluid power technology. This allows the user to easily parameterize even complex travel profiles, for example for forming and joining technology, injection molding machines and other applications that involve large forces. Apart from the standard function “Safe Torque Off”, IndraDrive drives offer further certified safety functions. With the help of “Safety on Board”, which is integrated in the drive, machine manufacturers can reach safety levels up to SIL 3 according to IEC 61508, which corresponds to PLe according to IEC 13849.

Stand-alone self-contained electro-hydraulic servo axis are characterized by their high energy efficiency. The servo-drive lowers the motor speed for the pump in line with the demand in partial-load operation or switches to stand-by mode, if temporarily no movement is required. Power branching in multi-axis operation is accomplished purely electrically. The controllers recover braking energy and can make it available to other consumers via an intermediate circuit. In addition, it is possible to store the recovered energy or feed it back to the mains.

Simulation for dimensioning in line with application requirements

For the rating of the SHA in line with application requirements, Rexroth developed a simulation program on the basis of experience in modelling of hydraulic systems gained over decades. This software tool shortens the time to market and offers machine manufacturers higher safety in the engineering phase.

Thanks to the modular design of the SHA with standardized sub-assemblies, the machine manufacturer can easily adapt the axis exactly to his application. SHA from Rexroth cover the power range from 100 kN to 2.500 kN in pulling and pushing direction. The maximum stroke of the axes, which feature protection class IP 65, is 1,800 mm. With an integrated, magnetostrictive absolute encoder, the accuracy is 1 µm.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, the company generated sales of 5.6 billion euros in 2014, according to preliminary figures.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, its roughly 290,000 associates generated sales of 48.9 billion euros in 2014. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its more than 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic goal is to deliver innovations for connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-07-18
Statement

Steel, rubber and oil – digital?! Industrial hydraulics must pick up the pace on the way to the digital future

Industrial hydraulics – today, this largely amounts to standard hydraulics consisting of iron, rubber, oil and, maybe, 24V connection sockets. At the same time, Industry 4.0 and the Internet of Things are changing the face of the factory floor: Decentralized intelligence, integrated sensor technology and connectivity have already become key requirements for many industrial applications. Nonetheless, hardware-intensive industrial hydraulics is in a position from which it can smoothly glide into this new digital environment. The requirement: Hydraulic manufacturers must accept the challenge of intensively advancing digitalization.


2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow: