Press

Content
080-11 Lohr, 2011-08-17

Enables access to the workpiece from below

The new open center section

Open for more applications: The new open center section of the TS 5 transfer system from Rexroth enables access to the workpiece from below.

An open center section as new standard module provides greater application options for the TS 5 transfer system from Rexroth

The TS 5 transfer system from Rexroth sets heavy loads up to 300 kilograms quickly and efficiently in motion. Rexroth now offers a new open center section as a standard module that enables access to the workpiece from below. Users can implement both lift and rotate stations, as well as customer-specific positioning units. Automated processes such as tightening and test stations on the bottom side of the workpiece can be directly integrated in the material flow. This seamless system thus increases efficiency when transferring loads.

The TS 5 transfer system with king shaft convinces with its maintenance-free and low-noise operation, as well as high energy efficiency, based on its excellent overall efficiency. Depending on the workpiece size, customers can configure the roller conveyors in 455, 650 and 845 millimeter system widths. The system is designed to allow branching off beyond the drive side to the right or left, which simplifies planning considerably. The products are either transported on workpiece pallets or directly on the roller conveyor.

The new open center section offers a wide range of options for the direct integration of automated processes. Eliminating the need for specialized solutions, the open center section is now available to users as a standard module. For workpiece pallet transport, short rollers with bearings on both sides are implemented to ensure the system’s stability.

The drive concept provides plenty of freedom for customized configurations: The open section can be equipped with a king shaft on one or both sides. The drive on one side offers an especially economical solution for workpiece pallet weights up to 200 kilograms. For heavier applications or a highly offset center of gravity, the drive on both sides guarantees secure transport.

Users can easily and quickly configure their specific system with open and closed sections. Rexroth's MTpro planning software contains all components of the TS 5 modular system as 3-D models. Added reliability in planning is provided by defined interfaces which allow the free combination of all modules. The robust design of the TS 5 makes it suitable for applications in harsh environments and even machining.

Rexroth at the Motek in Stuttgart: Hall 3, booth 3305

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue in 2010.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros in fiscal 2010. For 2011, the company forecasts sales of more than 50 billion euros and a headcount of a good 300,000 by the end of the year. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Additional information can be accessed at www.bosch.com ,www.bosch-press.com

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de