Press

Content
019-11 Lohr, 2011-04-04

Create Pneumatic Circuit Diagrams Quickly and Easily

Even complex circuit diagrams can be easily created using the intuitive software

Even complex circuit diagrams can be easily created using the intuitive software

Rexroth offers new circuit diagram software with the D&C Scheme Editor 3.0

With the new D&C Scheme Editor 3.0, Rexroth presents a special offer for design engineers. Free of charge and with no licensing requirements, the circuit diagram software is highly intuitive and easy to use. It also permits the creation of complex pneumatic circuit diagrams in compliance with standards.

A comprehensive pneumatic symbol library provides the basis for the circuit diagram tool. Symbols can be easily taken from the library, placed on a worksheet using drag & drop, and connected to a complete circuit diagram. Frequently used symbols can be stored as favorites in a user-defined folder structure. This makes it even easier to create circuit diagrams.

Material numbers or designations can be used to search for individual products that are not represented as a circuit diagram symbol. Graphical objects, such as lines, circles and rectangles with many possible settings for colors and types, provide additional options for customizing the circuit diagrams. It is also possible to integrate text and images.

The components are aligned on a grid, allowing ports to be arranged according to the grid. The components can be rotated in 15° steps. For the individual components in the circuit diagram, the user can assign material and item numbers as well as accessories. Based on this model, parts lists can be generated, which can then be used to start the order process – an important function, both for the documentation and administration of a system. Additional data sheets can be used to expand the circuit diagram. Each individual object can also be hyperlinked to further documents – all in a single application.

No knowledge of CAD or CAD licenses are required to use the D&C Scheme Editor 3.0. The software is available in German and English and is compatible with the Microsoft operating systems Windows XP, Windows Vista and Windows 7. The software as well as corresponding documentation is available for download on the Internet at www.boschrexroth.com/dnc-scheme-editor .

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and using renewable energies. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2009 Bosch Rexroth part of the Bosch Group, achieved sales of around 4.1 billion Euro with 34,200 employees.

For more information please visit www.boschrexroth.com/press

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, some 283,500 associates generated sales of 47.3 billion euros in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 300 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some four billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Additional information can be accessed at: www.bosch.com , www.bosch-press.com

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de