Press

Content
103-10 Lohr, 2010-11-22

Precise and Fast

The new compact modules from the inline I/O family from Rexroth offer high measurement accuracy, imp

The new compact modules from the inline I/O family from Rexroth offer high measurement accuracy, improved control quality and faster cycle times.

New SERCOS III-I/O-Modules with High-Performance Capability from Rexroth

Input and output signals are processed quickly by the new compact modules from the I/O-family from Rexroth via SERCOS III. Extremely short response times and fieldbus communication with SERCOS III, allow the modules to offer high measurement accuracy, improved control quality and faster cycle times in the application.

SERCOS III Block I/O Fast Digital with IP 20 protection has 16 digital inputs and 16 combined inputs/outputs for connecting digital sensors or actuators in a housing. Whereby the latter can be used to treat each channel as an input or output, so that the I/O module can be easily adapted to meet specific requirements. Optimized input/output wiring enables typical delay times of no more than 50 µs.

SERCOS III Block I/O Fast Analog with IP 20 protection has six inputs and four outputs. All inputs and outputs can be configured individually. The six inputs are used for analog current or voltage signals. Current or voltage actuators can be connected to the four outputs. The differential current and voltage inputs are characterized by their high accuracy in particular, with 16-bit resolution and extremely fast process data operation. Both input and output signals are available in just 40 µs.

"Synchronous" mode can be selected in addition to "Fast Response" mode for both block I/Os to receive and transmit all inputs and outputs at a defined synchronization time. The values are then always provided in synchrony in the higher-ranking SERCOS III network.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and using renewable energies. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2009 Bosch Rexroth part of the Bosch Group, achieved sales of around 4.1 billion Euro with 34,200 employees.

For more information please visit: www.boschrexroth.com

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de