Press

Content
104-10 Lohr, 2010-11-22

The Right Controller for Every Requirement

The IndraControl L25 controller enhances Rexroth's portfolio of controllers for medium-power PLC and

The IndraControl L25 controller enhances Rexroth's portfolio of controllers for medium-power PLC and motion applications.

New controllers for PLC/motion and CNC applications from Rexroth

With the new IndraControl L25 and L85 controllers, Rexroth presents two additional hardware platforms for motion logic systems. Whereas the IndraControl L25 supplements the company's controllers for medium-power PLC and motion control applications, the IndraControl L85 meets very demanding requirements for CNC applications.

The new IndraControl L25 represents a further function and code-compatible platform for PLC applications in conjunction with the IndraLogic XLC system solution and for motion applications in conjunction with the controller-based IndraMotion MLC motion logic system solution.

The high-performance IndraControl L85 controller is a platform for CNC applications that is capable of meeting ultra-high requirements with respect to processing time. Equipped with a dual-core processor, the platform introduces an additional CNC performance class based on the CNC system solution IndraMotion MTX advanced. Intelligent distribution of resources on the CPU cores enables genuine parallel processing of CNC and PLC functions.

Both controllers feature communication interfaces as master or slave for SERCOS III, PROFINET RT, EtherNet/IP and PROFIBUS and support the same Inline I/O modules as the established control platforms of the IndraControl L series. Additional functions and auxiliary communication interfaces are provided as function modules.

The entire engineering workflow, including configuration of the controller, is defined uniformly in the IndraWorks software tool.

The new IndraControl L25 and L85 controllers integrate into existing automation solutions from Rexroth in a homogeneous and compatible manner.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and using renewable energies. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2009 Bosch Rexroth part of the Bosch Group, achieved sales of around 4.1 billion Euro with 34,200 employees.

For more information please visit: www.boschrexroth.com

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de