105-10 Lohr, 2010-11-22

Faster Automation Thanks to New Functions

IndraLogic XLC offers new functions, fast real-time communication via SERCOS III, and is ideal for a

IndraLogic XLC offers new functions, fast real-time communication via SERCOS III, and is ideal for a variety of applications.

New PLC family: IndraLogic XLC from Rexroth

With IndraLogic XLC (eXtended Logic Control), Rexroth presents a new family of PLC controllers whose capabilities go far beyond the familiar PLC standard functions.

Users can leverage a wide range of new functions that realize modular software projects quicker than before. All planning, configuration, programming and diagnostic functions are standardized in one single engineering environment. Flexible motion control functions are already integrated. IndraLogic XLC can be connected into different communication networks thanks to real-time communication via SERCOS III and other common communication interfaces.

IndraLogic XLC enables scalable, controller-based and embedded PC solutions in conjunction with the latest IndraControl device platform. IPC-based hardware variants will round off the device portfolio in 2011.

Rexroth advanced the PLC programming together with technology partner Smart Software Solutions (3S). The PLC basis kernel from CoDeSys V3 was integrated homogeneously into the IndraWorks software tool and the multitasking runtime system. This allows users to take advantage of many new functions that allow modular software projects to be created in an end-to-end overall system in less time than before. Functions include convenient editor tools, object orientation as an extension to IEC 61131-3, and comprehensive function libraries as well as fast compilers for efficient generation of machine codes. The modular GATcompact (Generic Application Template) project template simplifies the process of realizing new machines with enhanced software quality while reducing effort considerably.

End-to-end communication between the controller and decentralized system peripherals, such as inputs and outputs or drives, takes place via real-time Ethernet SERCOS III. Fast PLC cycles to 250 µs enable optimum response times for handling time-critical process signals. IndraLogic XLC controllers come with versatile motion control functions, integrated into the run-time systems, to enhance the previous IndraLogic systems.

Applications cover the simple commanding of single axes, to synchronization of multiple axes, through to integrating FlexProfile for implementing complex motion sequences. The graphical profile editor in the IndraWorks software tool offers numerous offline and online functions for this purpose.

Master and slave interfaces for PROFINET RT, PROFIBUS and EtherNet/IP are available, in addition to SERCOS III, to facilitate integration into a wide range of communication networks.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and using renewable energies. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2009 Bosch Rexroth part of the Bosch Group, achieved sales of around 4.1 billion Euro with 34,200 employees.

For more information please visit:


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573