Press

Content
PI 032-15 Lohr am Main, 2015-08-05

Configurable linear motion systems and ball screw assemblies in just a few days

Delivered from the factory after a maximum of ten working days: Individually configurable linear motion systems from the GoTo Focused Delivery Program by Rexroth.

Individually configurable linear motion systems are now also available in the GoTo Europe Focused Delivery Program

Rexroth is expanding the GoTo Europe Focused Delivery Program with its short delivery times to configurable linear motion systems and ball screw assemblies. The manufacturer guarantees shipment of the individually assembled modules from the factory after a maximum of ten working days. The Focused Delivery Program is comprised of the configurations that customers order most often.

Time is money, this is true in industry now more than ever. Due to large fluctuations in demand, industry companies are making investment decisions at short notice more and more often. This increases time pressure on manufacturers of machines and automation devices. The GoTo Europe Focused Delivery Program fulfills these response time expectations. Rexroth compiled the components that are ordered most often in linear motion technology into the GoTo Focused Delivery Program two years ago and delivers the orders within three to five days. Configurable linear motion systems have been added to this recently; these are delivered from the factory in ten days. The same applies for ball screw assemblies, which can be arranged individually by design engineers and purchasers, with different lengths, leads, end machining and nut types.

The Focused Delivery Program is summarized in the GoTo overview catalog. On Rexroth's website, design engineers and purchasers can use the online tools to configure their desired linear motion system according to their requirements: for every configuration item from the drive-unit options, either a ball screw or toothed belt drive, to the system length and effective stroke and the motor and motor mounting as well as the carriage type and sensors. During each step, the configurator shows whether the chosen product configuration is included in the GoTo Focused Delivery Program. The user can view data for all products and performance characteristics and receive the CAD data in all common formats via a download link.

In addition to linear motion systems, Rexroth offers a complete product portfolio from ready-to-install axes to multi-axis solutions for almost all assembly and handling applications in various industries.

Apart from linear motion technology, the GoTo Focused Delivery Program by Rexroth also includes hydraulics, electric drive and control technology as well as assembly technology with quick delivery times.

Link to the GoTo Focused Delivery Program for linear motion technology PDF catalog:

www.boschrexroth.com/goto-lt

Like to the linear motion system online configurator:

www.boschrexroth.de/config-ls

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 33,700 associates generated sales revenue of approximately 5.6 billion euros in 2014.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 360,000 associates worldwide (as per April 1, 2015). The company generated sales of 49 billion euros in 2014.* Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including its sales and service partners, Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic objective is to create solutions for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

*The sales figure disclosed for 2014 does not include the former joint ventures BSH Bosch und Siemens Hausgeräte GmbH (now BSH Hausgeräte GmbH) and ZF Lenksysteme GmbH (now Robert Bosch Automotive Steering GmbH), which have since been taken over completely.

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de



Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.