Press

Content
2015-08-27

That's how it is: six surprising capabilities of modern hydraulics

That's how it is: six surprising capabilities of modern hydraulics

Dr. Steffen Haack, Executive Board of Bosch Rexroth AG, responsible for Industrial Applications and Sales Division

Anyone gaining only a superfluous familiarity with fluid technology will easily underestimate the performance and intelligence of modern hydraulics. Who would think that this technology is highly precise, energy-efficient, and ready today for Industry 4.0 applications? Here are six capabilities of a strong drive technology, which probably come as a surprise for many:

Micrometer precision: electrohydraulic axis controllers close the control loop decentrally, similar to electrical servo drives, and harmonize the target/actual position in real time within milliseconds. The precision of the movement solely depends on the respective utilized measuring system. In tool and plastic machines, hydraulic drives reliably position axes to a few micrometers precise. (Image 1)

Compact: It is often difficult to place electromechanical drives with sufficient performance in tight construction spaces. Unlike hydraulic drives they also add significant heat. Since power generation is decentralized in the power unit and since it is connected to the actuator via lines or pipes, OEMs can generate high forces even on minimal construction space. The relatively low level of heat created in the work area dissipates optimally through the hydraulic fluid. (Image 2)

Need-based energy efficiency: Software combines the best from electrical and hydraulic systems. The decentralized intelligence in the electronic control device adjusts the rotational speed of the pump drive on demand as the consumer requires power, or it lowers it to zero. In comparison to common constant drives, this reduces the energy consumption of hydraulic power units by up to 80 percent. By the way: even older facilities and machines can be retrofit without major efforts to significantly reduce the energy consumption in production. (Image 3)

Balanced drive physics: Fluid technology is not always inherently linear. Drive software for hydraulic actuators takes these particularities into consideration and harmonizes them automatically. Preprogrammed, typical hydraulic functions, e.g. synchronization or position-dependent braking, merely require the optimization of parameters within the scope of start-up. They are based on a transparent software structure and function equally on all hardware platforms. (Image 4)

Open and outgoing: With increasing frequency, real time Ethernet protocols in modern machines integrate all actuators and peripherals into each other. Modern motion controls for hydraulic drives support all common protocols, e.g. Sercos, EtherCAT, Ethernet IP, PROFINET RT, Powerlink and Varan. Their software is also based on open standards, e.g. IEC 61131-3 and PLCopen. With this they are an ideal match for the increasingly integrated and technology-overlapping infrastructure of modern production environments - all the way up to Industry 4.0 (Image 5)

Simply exchangeable: Ready-to-install servo-hydraulic axes have an integrated fluid loop and are driven by the same servo drives as the electromechanical versions. Since axes are encapsulated systems, engineers must only connect power and communication cables for assembly and start-up, and start-up can begin. Everything else, for example the parameterization values determined from simulations, are already stored in the drive software and support the plug & run philosophy. (Image 6)

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de



Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-06-05
Press Information

Bosch Rexroth expands additive manufacturing

The topic of additive manufacturing is becoming increasingly important in the production of small series and prototypes, as well as in the area of Industry 4.0. Bosch Rexroth also believes in this future-oriented technology. The company worked with TRUMPF and Heraeus Additive Manufacturing to develop a further additive manufacturing process for the cost-effective production of hydraulic components. With a focus on the Selective Laser Melting method, the project involved the production of servo valves. As an additional standard procedure to conventional production this can be used above all for quick production of small batch sizes and customized variants. Bosch Rexroth already uses several 3D printers for the production of casting cores for control blocks in Lohr and has expertise in the entire process chain from engineering to 3D printing to the finished product.