Press

Content
PI 011-16 Lohr am Main, 2016-01-22

ActiveMover: Quick precision movement

Rexroth ActiveMover transfer system: workpiece pallet changeover times ranging from 0.1 seconds shorten cycle times in short cycle applications.

Rexroth's new transfer system with linear motors is quick, precise and able to deal with heavy workloads

With workpiece pallet changeover up to ten times as fast, Rexroth's new ActiveMover transfer system significantly increases productivity in short cycle applications. Linear motors with an integrated measuring system position the sturdy workpiece pallets very precisely on a closed type trackway using a powerful drive that provides a force of up to 160 N.

The transfer system consists of straight section and curve units with vertically installed low-wear linear motors. These accelerate workpiece pallets with forces of up to 4 g, making the system extremely dynamic. The maximum speed is 150 m/min. The changeover time for the magnetically coupled workpiece pallets ranges from 0.1 to 0.3 seconds, depending on their size. Users therefore achieve time savings of up to 90% compared to conventional transfer systems. In practice, they achieve productivity improvements of up to 20 percent by using ActiveMover – but without precision being compromised in any way: the ActiveMover workpiece pallets move into any chosen position with a repeatability of +/- 0.01 mm, which consequently enhances process reliability. The integrated measuring system means that no additional indexing is necessary.

Users can use as many workpiece pallets as they want on the straight section and curve units, and they can control them individually. The travel direction, speed, acceleration, position and process sequence of each workpiece pallet can be programmed as desired. Integrated collision control ensures safe operation. ActiveMover communicates via ProfiNet or Ethernet I/P with any chosen process control system, and it automates short cycle applications in a very flexible manner. In addition, the workpiece pallets are prepared for the integration of identification systems.

The transfer system combines the conveyor section and 180-curve units into a freely configurable closed trackway. The vertical arrangement of the workpiece pallets means that they can be easily accessed from any side. With a drive force of 160 N, they can carry a payload of up to ten kilograms. The holder width is up to 500 mm. Existing drilled holes simplify the installation of customer-specific workpiece holders. The system transports sensitive products very gently and it consequently caters for a wide range of installation applications in electronics manufacturing, the automotive supply industry, and the medical technology and life science fields.

The enclosed power electronics achieve a protection category of IP65. The predrilled holes in the sturdy frame made of painted steel facilitate the integration of processing stations and protective enclosures.

Economic, precise, reliable and energy-efficient: Bosch Rexroth drive and control technology is the motive force behind machinery and plant of all sizes. The company brings together its worldwide applications experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies to develop innovative components and tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear and assembly technology from a single source. With a presence in over 80 countries its workforce of more than 33,700 employees achieved sales of around 5.6 billion euros in 2014.

Further information available at www.boschrexroth.com

The Bosch Group is a leading global technology company and service provider with a worldwide workforce of roughly 360,000 employees (as at: 04/01/2015). In the 2014 financial year it generated sales of 49 billion euros*. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including its sales and service partners, Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2014, Bosch applied for some 4,600 patents worldwide. The Bosch Group’s strategic objective is to create solutions for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Further information is available at: www.bosch.com , www.bosch-presse.de , http://twitter.com/BoschPresse.

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-04-23
Press Information

Bosch Rexroth presents collaborative robot based on KUKA

Bosch Rexroth continues to expand its portfolio of Automatic Production Assistants (APAS): With the APAS assistant, the company now also integrates KUKA technology into its product range. Unique product features enable a simple and safe entry into the world of human-robot collaboration. Complete with capacitive sensor skin to avoid collisions, selectable control and the widely-used PLC interface mxAutomation, the six-axis robot is set to become the perfect link for combining the strengths of human and machine in the factory of the future.


2018-04-23
Press Information

IT-supported individual product assembly and process optimization

In the factory of the future, business and production processes are growing ever closer together. Bosch Rexroth supports the essential flow of data from IT to individual assembly stations and back from the production line to IT with the two system solutions ActiveAssist and ActiveCockpit. The intelligent ActiveAssist assembly assistant system guides employees through multi-variant assembly tasks all the way to batch sizes of 1. The interactive communication platform ActiveCockpit collects, filters and processes data from complete production lines in real time for systematic process optimization. Both system solutions are driving the evolution to the data-based factory of the future.