International
 

Press

Content
PI 036-16 Lohr am Main, 2016-04-11

A complete range: two new electromechanical heavy-duty cylinders from Rexroth

Ready-to-install electromechanical cylinders from Rexroth cover pressure and pulling forces up to 290 kN with two series: EMC and EMC-HD, offering a total of 12 sizes.

Robust assemblies for freely programmable motion sequences

With two new sizes 105 and 150, Rexroth has increased the scalability of the EMC-HD electromechanical cylinder for moving heavy loads in machines, plants and outdoor installations. In five power stages, the heavy-duty series covers pressure/pulling forces up to 290 kN. The robust, ready-to-install actuators comply with the IP65 protection class and can even withstand harsh environments. They are based on Rexroth's ball and planetary screw drive portfolio, which has grown over the past 30+ years. Movement profiles can be implemented energy-efficiently and with a high level of precision, no matter how complex they are.

Simply enter the parameters for force, speed or location and the EMC-HDs already start moving extremely heavy loads accurately and precisely according to the parameters of the controller. The electromechanical cylinders can be integrated flexibly into modern automation structures and greatly simplify the engineering as a ready-to-install assembly. With a maximum stroke of 1,800 mm, they can move to any number of positions chosen by the user. Even without an additional position measurement system, the EMC-HDs can achieve repeatability of up to ± 0.01 mm.

Even the standard version of the EMC-HD fulfills the requirements for the IP65 protection class. This means that they are suitable for outdoor use and perform reliably over a wide temperature range of -10°C to +60°C. In the versions with planetary screw drive and low-temperature grease, the working temperature may reach down to -30°C. The piston rod is corrosion resistant and can even withstand direct contact with water. The simple and robust structural design ensures a long service life even under harsh environmental conditions. The sealing system protects the cylinder from contamination from outside, which could lead to wear, and thus ensures longer intervals between preventive maintenance.

When it comes to the two new versions, users have the choice between high-precision ball or planetary screw drives from Rexroth with a range of leads and in different sizes. This allows force and dynamic performance to be matched to the requirements of the respective application. Rexroth offers the EMC-HD both as ready-to-install, purely mechanical axes and as a complete system with a choice of precisely matched gear units, servo motors and drive controllers from the IndraDrive series up to four megawatts.

In total, the Rexroth range of electromechanical cylinders includes 12 sizes. The smaller EMC series with aluminum housing begins with pressure/pulling forces up to 1.2 kN and extends to 56 kN in seven power stages. The five versions of the EMC-D heavy-duty cylinder with steel housing start overlapping at 44 kN and go up to 290 kN. Both series are suitable for universal use in nearly all applications for machinery and plant engineering.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 33,700 associates generated sales revenue of approximately 5.6 billion euros in 2014.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). According to preliminary figures, the company generated sales of more than 70 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at roughly 115 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de