Press

Content
PI 033-16 2016-04-25

IMS-A Integrated Measuring System From Rexroth: Absolute, Inductive and Precise

Guide and measuring device in one: The IMS-A integrated measuring system captures the absolute position inductively with a high degree of precision, even under mechanical loads and in polluted environ

Linear guides with absolute value recording as accurate as glass scales, but more robust

Whether in machining operations, 3D printing or electronic handling - ever greater accuracy and availability are essential. The new Rexroth IMS-A measuring system, which is integrated in linear guides, is helping to achieve just that. It detects the absolute position of the axis to +/- 4 micrometers. What's more, the measuring system is immune to contamination, vibrations, shocks and magnetic interference and needs no buffer batteries in the event of a power failure. Thanks to the complete integration of the sensor and evaluation electronics in the ball and roller runner blocks, design engineers can avoid external measurement systems and air purge systems.

Turning machines back on again following a power failure can result in a critical situation. The controller in many applications needs to know the position of each axis immediately. Purely incremental measuring systems need to first complete a reference run for this. This extends the ramp-up time and, in a loaded state, can result in damage to the workpieces and tools. The new integrated IMS-A measuring system from Rexroth immediately recognizes the absolute position of the axis with a high degree of precision when the machine is switched on and reports them to the controller without carrying out a reference run. For this, the system does not require buffer batteries that need to be replaced regularly.

Inductive and wear free

Thanks to the inductive measuring principle, the IMS-A operates without physical contact and is therefore a wear-free assembly. The measuring scale cannot be interfered with or destroyed by external magnetic fields. The IMS-A is not sensitive to vibrations up to 10 G and shocks up to 50 G. The sensors and evaluation electronics are located in protective housing on the end face of the runner block. Even in working spaces with coolants, dust, shavings and other contaminants, the IMS-A does not require elaborate energy-eating, high-maintenance air purge systems. Even electrical and magnetic interference fields do not affect the measurement results. This ability makes the IMS-A destined to also be combined with linear motors, for example. Here it combines precision with high dynamic performance requirements and gains the full dynamics of ball and roller rail systems from Rexroth. The permissible acceleration is up to 500 m/s² and the maximum speed is 5 m/s, or even up to 10 m/s upon request.

Precision machining

With the IMS-A, position detection takes place very close to the tool center point, an important prerequisite for high precision, and thus surface quality in machining. The position resolution of the IMS-A is up to 0.025 µm. This extremely low value creates the conditions for excellent control loop dynamics and thus short cycle times. The system accuracy of +/- 4 µm/m lies within that of glass scales. This means that repeatability of +/- 0.25 µm is possible.

Integrated functions

The functional integration of guiding and measuring in an assembly minimizes installation times. No adjustment of the measuring system is necessary. With the IMS-A, engineers can use several runner blocks on an up to 4,500 mm long profile rail independently and without any accuracy limitations. All components, i.e. rail, runner block with adapter plate and scanner, are individually replaceable in the event of servicing. This reduces servicing costs. The interchangeable construction offered by Rexroth ensures even less effort. All runner blocks of the same size fit onto the profile rails of the respective size without any restrictions. The measuring system transmits the data via HIPERFACE© (*) interfaces, as well as via SSI/1Vp-p to the intelligent drives or controller. DRIVE-CLiQ (**) and FANUC interfaces are to follow.

Prepared for Industry 4.0

The integration of additional temperature and motion sensors makes this measuring system prepared for the future requirements of Industry 4.0. The additional sensors allow machine designers, for example, to read out the temperature and the actual dynamics. The sensor data also forms the basis for future approaches to predictive maintenance. The user can record and evaluate operating states online. If the accelerometers detect changes, such as increasing vibrations, then this is an indication of wear or other problems. Scheduled maintenance can then intervene before the machine needs to be shut down.

(*) HIPERFACE© is a registered trademark of Sick Stegmann GmbH

(**) DRIVE-CLiQ is a protected trademark of Siemens

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 33,700 associates generated sales revenue of approximately 5.6 billion euros in 2014.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). According to preliminary figures, the company generated sales of more than 70 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at roughly 115 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.