Press

Content
PI 035-16 Lohr a. Main, 2016-05-04

Linear bushings for application temperatures up to 200°C

Universally applicable: Linear bushings and linear sets from Rexroth.

For ambient conditions up to 200°C Rexroth has added all-steel linear sets to its product range. These and many more new developments enhance Rexroth's circular guide program. The new "linear bushings" product catalog provides an overview of the entire range.

Whether in foundries, tempering furnaces or other thermal processes: Guides with plastic parts reach their limits wherever there are high ambient temperatures. That is when linear sets made completely of steel from Rexroth are called for; they can withstand ambient temperatures of up to 200°C indefinitely. This consistency in the material also makes the product suitable for processes whereby conventional synthetics negatively impact process safety.

Rexroth also offers suitable, induction-hardened and ground precision steel shafts up to 80 mm in diameter for all temperature-resistant, ready-to-install linear-set models. Whether as a solid or hollow shaft, made of heat-treated steel, or with corrosion-resistant finish or hard chrome plated, they can be used for a variety of different tasks. Rexroth also offers customer-specific processing of the shaft ends up to a diameter up to 110 mm.

What's more, Rexroth has also developed open-type super linear bushings with 20% higher capacity thanks to the symmetrical arrangement of the rows of balls. Compact ball bushings in even smaller sizes, as well as corrosion-resistant versions round off the extended product range.

Rexroth provides a clear overview of the full and comprehensive program in the new linear bushing guides catalog (R999000488). For an initial overview, please visit our website at www.boschrexroth.com/KBF. Many linear bushings and linear sets are also part of the GoTo preferred delivery range. Many linear bushings and linear sets are also part of the GoTo preferred delivery range with a standard shipping time of 3 days or less.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 33,700 associates generated sales revenue of approximately 5.6 billion euros in 2014.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). According to preliminary figures, the company generated sales of more than 70 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at roughly 115 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.