International
 

Press

Content
, 2016-05-17

Bosch Rexroth modernizes Eiffel Tower hydraulics

Hydraulics

Close to the original technology of the iconic Eiffel Tower, but with modern components state-of-the-art: Bosch Rexroth modernized the hydraulics for the elevator in the west pillar.

Construction true to the original with modern components and intelligent system design uses 25 percent less energy

The Eiffel Tower stands, seemingly unchanged, as the icon for Paris for now more than 125 years. But underneath the steel grid construction, the operating company SETE brings engineering up to date in order to reduce maintenance while increasing availability and energy efficiency. Simultaneously, each measure is to be as close as possible to the original technology. Bosch Rexroth, experienced system partner for the modernization of drive and control technology in historic facilities, updated the hydraulics of the elevator in the west pillar. In doing so, the company maintained the original construction idea of an indirect hydraulic drive and implemented it with current engineering. This reduces energy consumption by approximately 25 percent.

For forty years, the Eiffel Tower – built in 1889 with initially 312 meters – was the highest structure in the world. The builder and operator Gustave Eiffel focused on various elevator versions early on in order to enable as many visitors as possible to enjoy the view from the Eiffel Tower. Ten years after the opening, he advertised for bids for new, hydraulically operated elevators for the east and west pillars, because the functionality of the original solutions was not satisfactory. The elevators do not rise vertically to the second platform at a height of approx. 115 meters but follow the inclination of the pillar. An indirect hydraulic drive was therefore the only option. The engineers back then developed a unique mixture of hydraulic drive, high-pressure cylinders, mechanics, and cable pulleys. The elevator was retrofit in 1986 and the original construction was partially replaced.

When advertising for bids for the modernization project in 2008, the operating company Société d’Exploitation de la Tour Eiffel, SETE, searched for a solution that follows the construction of 1899 as closely as possible while fulfilling current safety standards, reducing maintenance, and increasing energy efficiency. Bosch Rexroth took on the modernization of the hydraulics. In the process, the engineers first had to reconstruct the original solution with the help of only partially preserved construction documents. Unlike more than 100 years ago, they were able to use the simulation program SIMSTER developed by Rexroth, which they used to mathematically verify the static and dynamic behavior of the overall system of hydraulics, mechanics, and electronics. In doing so, they guaranteed the dimensions and functions of all hydraulic components as well as the overall system even prior to production.

The modernized system again uses the original configuration with two lift cylinders and three high-pressure cylinders, which store energy when lowering the cabin and then provide this energy during upwards movement. The only major change – for reasons of energy efficiency – is the replacement of valves to control the up and down movement with displacement pumps, which were not yet available back then. With the modernization, Rexroth ultimately reduces the energy demand of the elevator by approximately 25 percent in comparison to the historic solution.

On the outside, the modern engineering is invisible. The cabins of the west elevator remain unchanged. The overall hydraulics are located in the underground engine room. In addition to the new, active components, some original components remain – although without – function. This gives the pump room a realistic impression of engineering of the late 19th century.

The modernization, which was completed in 2014, is one of a multitude of major projects, which Bosch Rexroth has realized worldwide as system partner or as general contractor. For example the company has updated the hydraulic equipment of the Tower Bridge in London to current state-of-the-art. During the complete renovation of the Bolshoi Theater in Moscow, Bosch Rexroth installed stage technology equipment that is worldwide among the most modern and most complex.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31,100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2021-04-12
Press Information

Bosch Bosch reveals fast and power-dense Hägglunds Atom hydraulic motor

The smallest of the Hägglunds hydraulic motors from Bosch Rexroth has been transformed. The Hägglunds Atom takes over from the existing Hägglunds CAb – supplying not only more revolutions per minute, but also far more power than motors of similar size. The result is a tiny, power-dense package ideal for mobile, marine and recycling applications.


2021-03-23
Press Information

Parameterizing and reading out hydraulic valves with a smartphone and Bluetooth

With the newly developed generation of digital on-board electronics for hydraulics, Rexroth allows economical scaling between analog components and those with a fieldbus/Ethernet connection. It takes advantage of the economic benefits of digitalization with no additional cabling. The new generation provides the open interfaces Bluetooth and IO-Link. In conjunction with a suitable app, commissioning engineers, operators and service technicians can access components and change parameters using their smartphone – directly and independently of the machine control system.