Press

Content
PI 046-16 Lohr am Main, 2016-05-31

Small and robust: compact pressure sensors up to 600 bar

New PR4 series 10 pressure sensors from Rexroth: only 55 mm long, they fulfill the IP67 and IP69K types of protection.

Rexroth's new generation of robust and precise pressure sensors

For fork lift trucks, telehandlers and other logistical vehicles, the trend is definitely moving toward more power in a smaller installation space. Rexroth is supporting this development with its new PR4 series 10 pressure sensors. In implement hydraulics and travel drives they cover measuring ranges of up to 600 bar with a length of just 55 mm. The sensors can be easily installed using a socket wrench with a tightening torque of up to 45 Nm.

The PR4 pressure sensors can be used universally in open and closed hydraulic circuits and deliver decisive information for energy-efficient power control. With three variants, the new series covers pressure ranges from 0 to 280, 0 to 420 and 0 to 600 bar. The pressure sensors can withstand pressure peaks of more than 130 percent of the nominal pressure; in the version for the highest pressure stage they can momentarily withstand up to 800 bar. Assembly with M14 or G1/4 threads is easy using a socket wrench with a high tightening torque of up to 45 Nm, as is often required with compact gearboxes, for example.

The sensors come from Bosch's large-scale production for the automobile division and are available long term. The hermetically sealed measuring channel guarantees high media resistance. They fulfill the IP67 and IP69K types of protection and offer high shock and vibration resistance. The total length is only 55 mm. The sensors are approved for an ambient temperature range of -40 to +100 °C. They can therefore also be placed in close proximity to the diesel engine. The permissible temperature range for the measured medium is -40 to +150 °C.

The measuring characteristic curve is linear. The ratiometric output signal covers the spectrum between 0.5 and 4.5 V, with a supply voltage of 5 V. A simple fault diagnosis can take place by checking this signal range. In the typical operating range for mobile working machines, the total accuracy of the PR4 pressure sensor is ≤ 1.1 percent of the nominal pressure over the entire pressure range during the complete service life. This accuracy improves the control quality of the hydraulic systems. The sensors fit seamlessly into the Rexroth modular system with mobile electronics and mobile hydraulics.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-06-19
Press Information

Transport and positioning perfected: linear motor-driven transfer systems from Rexroth

For the highly dynamic transport and exact positioning of materials and workpieces, linear motor-driven transfer systems are the first choice. Bosch Rexroth is enriching this market segment with two innovative solutions at once, and can therefore meet the specific requirements of series and special machine manufacturers alike. Customers looking for a quickly applicable system for short-cycle applications will find the perfect execution in ActiveMover. Those who require a high degree of freedom in design and programming, however, should opt for the flexible transport system (FTS), which, due to its modular principle, can be scaled individually.


2018-04-23
Statement

We take „Big Data“ and turn it into „Smart Data“

The Internet of Things, Connectivity and Industry 4.0 can no longer be considered hype. IoT is undeniably the trend, which will make the “Factory of the Future” a reality. To realize this, you only have to visit the Hannover Fair this year which takes place at the same time as CeMAT.