Simply collecting data is not enough!

Dr. Steffen Haack

How industry can gain valuable insights through machine learning

Dr. Steffen Haack, Member of the Executive Board with responsibility for the Business Unit Industrial Applications and Coordination Sales of Bosch Rexroth AG

“Soon it will be possible to connect everything. Components and machines are being equipped with additional sensors and higher performing controls. This means more data is available in manufacturing.

The mountain of data is growing. But what use is it? Manufacturing data should be a means to an end. The manufacturing information we collect must create added value. How can this succeed? The right data must be collected, connected together intelligently, analyzed and the right conclusions drawn, as quickly and as comprehensively as possible.

The IT industry shows the way: suggestions in search engines, webpages that offer related articles, language detection in your smartphone are all things internet users see every day. This isn't magic, it's mathematics. Algorithms learn relationships, group users and then generate suitable suggestions.

Machine learning makes use of self-learning software to process enormous amounts of data in the shortest time possible. A widely used approach is to use artificial neuronal structures that imitate the human brain. In this way complex relationships can be recognized, learned and reproduced, where rules-based "if/then relationships" only scratch the surface and simple programs fail.

New knowledge for complex manufacturing processes

For the manufacturing industry, this method contains enormous optimization potential. For example, it can be used to more easily plan complex manufacturing processes, reduce the energy consumption of machines or increase machine availability with preventative maintenance. Currently, automation technology companies offer solutions that allow operating statuses to be visualized online and make different kinds of data available. But this is just a first step.

With machine learning, software can detect wear patterns and its effects on manufacturing systems. Bosch Rexroth already uses this method for preventative maintenance of systems with very high standstill costs, such as in steel plants, paper factories or offshore installations. Numerous sensors in and on all critical components and modules continuously record operating data. This data is sent to a cloud where status information is calculated, drawing on data from all connected systems. With every data set, the software is better able to recognize patterns and the prediction accuracy for wear and potential failure increases continuously.

Knowledge of machines a requirement

Creative programmers with machine learning and domain knowledge, so-called data scientists, need to transform mechanical engineering and process know-how into a new generation of software. Without the knowledge of which kinds of components the data comes from, or when maintenance was performed on a machine, for example, the software cannot produce any useable results. The principle is self-evident: the more comprehensive the data set, the greater the potential use for all involved.

With cloud-based machine learning, data protection plays a decisive role, since Industry 4.0 can only be put into practice with the trust of customers. This is an important requirement in order to profit from new findings obtained from the data. At Bosch Rexroth we take great care with the data of our customers and we explicitly seek approvals for which data we can use for which purpose. Processing of the data is done on Bosch serversfully equipped with the latest, state-of-art data protection capabilities.”

ODiN Condition Monitoring

More information about Bosch Rexroth under:


Search press releases


Johanna Rauch
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1358

Related Articles

Press Information

Intelligent hydraulics for increased availability

Connected hydraulics increase the availability of machinery and plants through condition monitoring and predictive maintenance. For this purpose, Rexroth offers scalable solutions, from individual units with local evaluation to the complete, cloud-based monitoring of large plants. Sensors measure all relevant operating conditions and software detects wear before it leads to failure. Retrofitting kits also economically integrate already installed plants into these concepts.

Press Information

Linear motion, short time to market

Stand-alone linear axes are the trend. The combination of electrical drive unit and mechanical or hydraulic cylinder reduces installation space and engineering time and combines our specific professional knowledge in one system. With ready-to-mount and i4.0-enabled solution packages, Bosch Rexroth is in line with the current market requirements regarding electrification, digitalization and monitoring as well as condition-based maintenance. The uniform control and drive concept which is used in the different technologies serves as a basis for a short time to market and the economical implementation of hybrid solutions.