Press

Content
PI 070-16 Lohr am Main, 2016-09-20

VarioFlow plus expands application range

Rexroth VarioFlow chain conveyor system plus

The upgrade of the Rexroth VarioFlow chain conveyor system plus enables diverse applications, from general machine interlinking to food & packaging and electronics, through to transportation tasks

The time and cost-saving Rexroth chain conveyor system ensures competitiveness by enabling fast time-to-market

  • New drive and chain variants for a wide range of applications
  • Powerful ESD system in two sizes
  • Pre-designed, drop-in modules simplify project planning and assembly

With the upgraded modular system of the VarioFlow plus chain conveyor system, Rexroth now offers users a series of standardized solutions for specific conveyor functions, which simplifies the fast implementation of customer-specific designs. The application spectrum now includes everything from simple machine interlinking to special ESD solutions in the electronics industry, as well as secure transportation tasks in abrasive environments and stainless steel designs for food & packaging.

In virtually every industry, a competitive advantage depends heavily on short time-to-market. Rexroth’s VarioFlow plus chain conveyor, thanks to its ability to achieve easy and fast implementation of diverse, complex transportation tasks, provides an ideal basis for faster product introduction. The system enables flexible, customized solutions, saves space and is low-noise. In addition, the MTpro planning software supports fast project planning and with it, the ability to make short-term adjustments to changing market requirements.

With the latest upgrades to the offering of this modular system, users can now benefit from VarioFlow plus in the area of sensitive electronics production, as well. The ESD system ensures the safe avoidance of electrostatic build-up, offers a high chain tensile strength of up to 600 newtons and can also be used in applications requiring workpiece pallet systems.

For use in abrasive environments, the system now includes new compact clean-rated conveyor section profiles in stainless steel and stainless steel slide rails. They ensure that falling particles capable of causing extreme wear are carried out of the system immediately. Moreover, users can transport sharp-edged products directly on a steel-plated conveyor chain.

The new drive concept contains a center drive and a transmission kit, with which a direct drive can easily be upgraded to a transmission drive. Rexroth offers a low-cost solution especially for accumulating buffer applications: with the 90° return unit, users can significantly reduce the need for return chain. New chain types also ensure safe transport of a wide variety of products: the flocked chain protects delicate component surfaces, the gray chain minimizes optical distractions, and roller cleats protect product surfaces in ascending and descending conveyor sections.

Based on comprehensive application know-how, Rexroth has developed drop-in solutions for specific conveyor functions, such as a mechanically-controlled traffic barrier for conveyor section junctions. These ready-to-use components simplify the implementation of customer-specific systems for the user, without the need to spend great effort on planning.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

 

Search press releases


Contact

Johanna Rauch
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1358
johanna.rauch@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.