Press

Content
PI 071-16 Lohr am Main, 2016-09-29

Increased productivity and product quality through linear motor-driven transfer systems

Pallet Booster

Bosch Rexroth will present the application solution for short cycle times for the first time at MOTEK 2016. The demonstrator consists of the new pallet booster, guide module and belt section.

Rexroth develops a new application solution for short cycle times with the pallet booster

  • Innovative pallet accelerator combines technical advantages
  • Precise, quick and flexible transportation by linear motors
  • Application-specific system selection from a single source

With a focus on higher assembly system productivity, Rexroth developed the application solution pallet booster WB2 to reduce cycle times. The booster lowers unproductive workpiece pallet changing times to a minimum: Used in combination with the Rexroth TS 2plus transfer system, it accelerates the transport and brings the products onto the same workpiece pallet for the next processing step. As a specialist for transfer systems, Rexroth now presents further solutions for the realization of shorter cycle times with the booster to complement the ActiveMover and Linear Motion System (LMS). The Rexroth specialists can therefore always tailor and offer the appropriate solution concept according to the project.

The new pallet booster WB2 is a modular supplement to the transfer system TS 2plus. Unproductive time for the transport between individual processing stations can be significantly reduced with the booster as it is up to ten times quicker than the standard speed, depending on the application, with accelerations of up to 3g. The booster is used in the process station area. The system allows for the consistent use of the workpiece pallets without adaption into the entire system and their takeover "on the fly" on linear motor-drive conveyor units. This reduces the cycle time, above all in systems where products must approach a high number of different process stations especially quickly and flexibly.

In addition to productivity, the pallet booster also increases the product quality due to its high repeat accuracy. The individual workpiece pallets are automatically positioned by a linear motor. Thanks to the flexible control, sequentially cycled travel, travel in a group and reversing is possible. The precise positioning is done without additional indexing, which means that positioning units and other handling system are not required. As a standardized and preconfigured assembly, the pallet accelerator is completely compatible with the TS 2plus and can also be easily retrofitted into the transfer system, which saves assembly time and costs.

At MOTEK 2016, the international specialist trade show for production and assembly automation, Rexroth will present the application solution using a demonstrator for the first time, which consists of a guide module, belt section and pallet booster. Users receive the booster tailored to their individual application conditions from the Rexroth project department.

Rexroth offers further alternative solutions with the ActiveMover transfer system and the Linear Motion System (LMS), which are specifically targeted towards short cycle times. The ActiveMover is a convincing linear motor-driven circulation system with the shortest change times of 0.1 s and accelerations of up to 4 g, which increases productivity in short-cycle applications. The complete system is suitable for the transport of delicate products up to 10 kg and wherever high precision is required. With the flexible LMS modular system, numerous solutions can be realized with loads of over 1000 kg and in demanding environments such as in a vacuum. Rexroth therefore has different solution variants in their portfolio depending on the application requirement in order to be able to offer the optimal system according to the project.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

 

Search press releases


Contact

Johanna Rauch
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1358
johanna.rauch@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.